Other Parts Discussed in Thread: TVP5151, OMAP3530
I have a tvp5151 connected to an omap3530 - only d0-d7, HS, VS, and PCLK. Trying to work in bt656 mode.
I'm using a 2.6.32 kernel with the isp driver lifted from the 35x EVM (Mistral board) support.
No change to the register programming of the isp from the evm board and the 5151 is being programmed with 0x0d to the MISC_CTL (0x03) register and 0x47 to the MISC_CTL (0x30) register - everything else default.
My symptom is I can only get HS_VS interrupts. I have tried every combination of HS,VS,PCLK, and DATAPOl with no change. I never get a CCDC_VD0 interrupt.
An oscilloscope shows all the signals behaving properly (data changes when waving hand iun front of the camera), but every symptom poiints to the ISP not seeing data.
Any pointers?