Other Parts Discussed in Thread: AM3359
Hello,
I am having some problems creating a new project for my Beaglebone from the CSS5, using starterware.
For the beginning, I compiled the gpio (LED blink) example, put it on SD card and it worked. Then I tried creating a new CSS5 project for the AM3359, put the same gpio LED blink code in, set the include paths, set the post-build instructions... and build fails due-to unresolved symbols. Naturally, the linker does not know where to find the gpio and clock functions. How do I tell the linker, where those functions are? I've looked through the example project for the LED blink, and there are no linking instructions inside, which is kinda weird.
Annother strange thing happened when I've tried to put all driver files into my new project. I've copied in:
- gpio_v2.c
cache.c
clock.c
cp15.asm
cpu.c
exceptionhandler.asm
init.asm
interrupt.c
mmu.c
startup.c
And after that the project did compile and create .bin and _ti.bin. The problem is that the application does not work; the bootloader starts but then the LED does not blink.
I would be very happy for any suggestions on what to do.
Thanks to all.