This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6747 EMIFB sdram interface, series termination required?

Hello,

I am working on a C6747 schematic design, using the EVM schematic as a reference. I notice the EVM board uses series resistors on all sdram signals. I did not find any recommendations for such in TI technical reference literature. I remember a design from many years ago on the Intel StrongArm processor where series resistors were required on address lines, however of my more recent sdram interface designs series resistors have not been required or even suggested. There are downsides to using series resistors, mainly the additional solder connections and vias required, as well as having to break the signals to the surface rather than a clean run straight to memory on an inner layer.

Does anyone have any information or guidance they can share in this regard?

Thanks,

Steve