Hi all,
When we read source code of gralloc.cpp for gralloc.default.so which is in /system/lib/hw, we found gralloc_alloc function definition is as following. From folloing bold sentences, format is fixed as RGB, RGBA, RGBX for gralloc.default.so. For output port buffer of OMX decoder, its format is HAL_PIXEL_FORMAT_TI_NV12 which equal to 256.
So is there other method to malloc GPU memory for TI format? Thx.
static int gralloc_alloc(alloc_device_t* dev,
int w, int h, int format, int usage,
buffer_handle_t* pHandle, int* pStride)
{
if (!pHandle || !pStride)
return -EINVAL;
size_t size, stride;
int align = 4;
int bpp = 0;
switch (format) {
case HAL_PIXEL_FORMAT_RGBA_8888:
case HAL_PIXEL_FORMAT_RGBX_8888:
case HAL_PIXEL_FORMAT_BGRA_8888:
bpp = 4;
break;
case HAL_PIXEL_FORMAT_RGB_888:
bpp = 3;
break;
case HAL_PIXEL_FORMAT_RGB_565:
case HAL_PIXEL_FORMAT_RGBA_5551:
case HAL_PIXEL_FORMAT_RGBA_4444:
bpp = 2;
break;
default:
return -EINVAL;
}
size_t bpr = (w*bpp + (align-1)) & ~(align-1);
size = bpr * h;
stride = bpr / bpp;
int err;
if (usage & GRALLOC_USAGE_HW_FB) {
err = gralloc_alloc_framebuffer(dev, size, usage, pHandle);
} else {
err = gralloc_alloc_buffer(dev, size, usage, pHandle);
}
if (err < 0) {
return err;
}
*pStride = stride;
return 0;
}
regards,
guangx