I have configured my 6678l EVM to the default switch settings. I have tried running both the client NDK example and the hello world NDK example. I am currently getting this as output:
[C66xx_0] QMSS successfully initialized
[C66xx_0] CPPI successfully initialized
[C66xx_0] PA successfully initialized
[C66xx_0]
[C66xx_0] TCP/IP Stack Example Client
[C66xx_0] Configuring DHCP client
[C66xx_0] PASS successfully initialized
[C66xx_0] Ethernet subsystem successfully initialized
[C66xx_0] Ethernet eventId : 48 and vectId (Interrupt) : 7
[C66xx_0] Timeout waiting for reply from PA to Pa_addMac command
[C66xx_0] Add_MACAddress failed
[C66xx_0] Error: Unable to register the EMAC
[C66xx_0] NIMUIOCTL Failed with error code: -22
[C66xx_0] Service Status: DHCPC : Failed : : 000
[C66xx_0] Service Status: Telnet : Enabled : : 000
[C66xx_0] Service Status: HTTP : Enabled : : 000
Why am I unable to register my EMAC? Do I need to set a switch to a certain position to enable the on-board RJ45 connector?
THanks,
Will