This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

trouble linking dsplib.a674

I am trying to use the C6748 DSPLIB with CCS v5.2.  The compiler is happy with the include path that I provided for the required header files, but the linker is not finding the library or is not recognizing it.  The linker command options per my project configuration is the following:

-mv6740 -g -O2 --define=c6748 --define=CHIP_c6748

--stack_size=0x800 --heap_size=0x800 --warn_sections --display_error_number

-i"C:/ti/ccsv5/tools/compiler/c6000_7.3.4/include"

-i"C:/ti/ccsv5/tools/compiler/c6000_7.3.4/lib"

-i"C:/Program Files/Texas Instruments/dsplib_c674x_3_1_0_0/inc"

-i"C:/Program Files/Texas Instruments/dsplib_c674x_3_1_0_0/packages"

-i"C:/Program Files/Texas Instruments/dsplib_c674x_3_1_0_0/lib"

--reread_libs --rom_model

The last 3 paths specified are valid on my system, and the library that I specified in the configuration is "dsplib.a674" (this library is located at the last path specified).  I also tried specifying "dsplib.ae674", but that did not work either.  I'm not sure why "-l"dsplib.a674" does not show in my command line, but -l"libc.a" does not show in the command line either, and symbols are being resolved from that library.

Not sure what I am missing here.  Any suggestions?