Hi Ti Folks,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ti Folks,
Hi, RC:
No, the Pa_simpleExample should work in all boot modes. My test platform is always set to ETH boot mode. I have tried to run the same test at the latest 6670L and 6678L EVM and the example worked at both platforms.
Here is the proceude:
- Launch CCS v5.1.(0.0.00031)
- Launch the ccxml file (attached)
- Tools->GEL (load GEL evmc6670l.gel)
- connect core0
- system reset
- Scripts->LC_EVM_C6670_Functions->Global_Default_Setup
- Load the test project
- Run the test project
Best regards,
Eric