This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

am335x ZCE and USB



Hi.

We are using the am335x ZCE package (13x13mm), which only has one USB PHY. I'm working with the Sitara Linux SDK (psp04.06.00.08).

I'm having problems getting the mass storage function working. Neither the deprecated 'g_file_storage.ko' driver or the new 'g_mass_storage.ko' driver seems to work.

The TRM mentions that the unbonded PHY has to be set in HOST mode, SUSPEND state and USB_CTRLx register needs certain bits set.

Do I need to configure the USB driver somehow for this to happen or has support for the ZCE package not been implemented in the SDK yet?

br.

Nikolaj