Hello,
I am using DM365 based IP camera with IPNC 3.0 release files.
I am trying to check advanced features like motion detection face detection etc.
In case of motion detection. I enabled the appropriate motion detection setting and also alarm settings for logging. And found following issues
1. I found that system log gets updated some times and does not get updated most of the times.
2. If I keep motion detection enabled, after some time streaming screen goes black. (or sometimes streaming stops ie showing some still image)
And in case of face detection, I am not able to see the rectangle drawn in front of faces detected. (even after doing appropriate setting, also enabling region of interest)
Can anybody suggest if I have missed some important step in face detection feature ?
The most important thing is, we are using IPNC 3.0 release version but we are using IMX035 sensor (From sony).
Released IPNC 3.0 is not having support for this sensor, so we ported driver of IMX035 from IPNC 2.6 release to IPNC 3.0 release.
Could this be the reason for malfunctioning if these features ?
Regards
Mahesh