Hi,
We have the DM385 skype demo running. I loaded the provided Skype demo images onto the IPNC demo following the instructions. With a couple tweaks, I am able to make Skype calls, but I am not seeing any video on the IPNC side.
As instructed in the set up documents, I have the IPNC connected to a television with an HDMI cable. I have also plugged in the audio port to see if sound is being received by the IPNC. Neither of these are successful. When the call is connected, the IPNC pops up a window showing the local video, but neither the TV nor a window shows the stream from the PC.
I have tried starting and stopping the received video, without success. Is there a setting to tell the IPNC to send the incoming video to the TV?
I do see the following on the console suggesting the video is received.
Send bitrate: Bitrate: average: 28219 kbits/secGetCodec= 0
Start Playback: Width = 640, Height = 480
********************** START PLAYBACK 640 x 480 *******************
Receive bitrate: Bitrate: average: 14 kbits/sec Send bitrate: Bitrate: average: 1657 kbits/secReceive bitrate: Bitrate: average: 423 kbits/sec Setting frame-rate 17
[m3video] Channel:0 inputframerate:30 targetfps:17
Requesting IDR Frame
Thanks.
Regards,
Quinn.