This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Sitara AM3352 Mystical DDR2 problem



 

The mystical DDR2 problem occurs at 720MHz CPU and 266MHz DDR when I have adjacent bytes flipping all bits, i.e. going from 0xFFFF to 0x0000. Problem disappears when I lower DDR clock to 200MHz. Previously I had told Cary I lowered CPU frequency also --- that does not seem to be required. Anyway, I am reviewing the TI docs on the DDR registers ---- really interesting stuff.