This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Question about DM6467 CMEM & Cache



Hi, friends 

I am using DM6467t. I used to set L2 to be alll SRAM without using DMA. So I think DSP's reading external memory speed is based on the external memory itself since L2 cache and DMA  unable.  To accelerate the reading speed , I want to use L2 cache.

I use CMEM to allocate a segment of memory 16M in size  at base 0x88000000,which is aligned to L2 cache line size. And I configure  L2 to be all cache, set MAR136 to be 1 which corresponds to 0x88000000 to 0x88FFFFFF.

But I  see no improvement when DSP reads CMEM memory.

 I am confused about the result. Dose L2 cache work for the segment  used in CMEM?  Or I missed something key to the L2 cache?

Can any one help me how to improve my reading efficiency?

Best regards

Xie