This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dm368 multiple usb serial issue



Hi, we are working on ti dm368, 

sdk version is dvsdk_dm365_4_02_00_06

kernel version is  2.6.23.17

when we connect 4 or more usb serial devices (such as 3g modems, or usb to RS232 serial converter) on the same usb 2.0 hub,

we can see the kernel found ttyUSB0 ,ttyUSB1 ,, etc.  seems all work well

and if we open the first  three serial ports, it also works well

but when we open the fourth serial ports, it can only send data,  while receive data will fail, from cat /proc/interrupt, we can not see the

usb interrupt when receiving data,

does anynon meet this issue before and found the solution? thanks a lot.