This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

cmem memory configuration in EZSDK CE examples

Hello,

In order to run the Codec Engine Examples the EZSDK Software Developers Guide indicates that cmemk should be installed as follows:

cmemk phys_start=0x94000000 phys_end=0x947fffff pools=20x4096,10x131072,2x1048576

Why cmemk is configured that way? 20 pools of 4Kb, 10 pools of 128Kb and 2 pools of 1024Kb (total: 3408Kb)

In addition phys_start is set to 0x94000000. To which address corresponds according to the EZSDK Memory Map? To the Linux memory? Why there are no specific memory regions for Codec Engine usage like C6Accel?

Regards,
gaston