Hello, I am trying to make a circuit board with C6713B BGA DSP and AIC23B.
I studied the schematics of 6713 DSK, Spectrum Digital uses two McBsps for one AIC23.
McBsp0 for Control interface to set up the AIC23, McBsp1 for audio interface for exchanging
digital audio(Data Rx and Tx). My problem is how to connect one AIC23 to one McBsp only because I
need to use the other Mcbsp to send data to a Modulator and recei ve Data from an
ADC. For example Use Mcbsp0 with AIC23B and Mcbsp1 with Modulador(Tx) and
ADC(Rx). Its possible not to use the CPLD and use another type of glue logic?, if
its so which could be that glue logic or do you have an example of how to make the
conections or schematics?. Suggestions or recommendations.
Best Regards,
Company Name: Cinvestav
Contact Name: Ricardo Orozco
Contact Phone: +52013357473800x6350
Contact Email: rorozco@gdl.cinvestav.mx
Address: Av. IPN # 2508
City and State: Distrito Federal, D.F.
Postal Code: 44280