I'm using the DM8168 PG2.0 and having problems with several USB hubs. We have an iomega usb hub that works fine, but several others cause the kernel (2.6.37) to crash and the z3 board we're using to reboot the moment the musb driver is loaded. One hub does not crash the kernel, but on bootup it causes the USB port it's connected to to not work. It works if I unplug the hub from the port it's connected to and plug it into the other port. It also works if I wait for the board to finish booting and then plug it in. I don't have any other devices connected to these hubs and these hubs work in other computers including linux computers.
Any suggestions?