I have a custom DM8148 board, the HDMI circuitry is identical to the EVM.
Now when I plug in a HDMI display, the HPD pin stays low.
The same display works well with the EVM.
I use a micro HDMI connect instead of full size one.
I dont see any waveforms on the data pins either, but I guess that's the result of undetected display.
I tried several PCBs with same result.
Any suggestion or wild shot is greatly appreciated.