Hi all,
I've an issue in udp receiver on OMAPL138 using NDK version "2_20_00_19" and bios version "5_41_10_36".I'm using another OMAPL138evm having same NDK but with bios version "5_41_07_24" to sent data using sendto() function,which is running flawlessly
i.e, EVM to EVM communication in which Tx part is working fine but Rx end is crashing after some time(nearly after 6 minutes everytime)
can anyone give an insight on cause of this problem...
-Thanks