Other Parts Discussed in Thread: SYSBIOS
Hi,
I'm currently trying to rewrite interrupt functions in a C6670 project to use SYS/Bios instead of the CSL Intc .
Most of the stuff worked fine, but now I have an interrupt that gets called by an Event Combiner event.
I want to rewrite this event combiner interrupt to use SYS/Bios i.e. ti.sysbios.family.c64p.EventCombiner
static CSL_IntcRegs *IntcRegs = (CSL_IntcRegs *) CSL_CGEM0_5_REG_BASE_ADDRESS_REGS;
// combined event to know which incoming EDMA gets triggered
interrupt void
Aif2_RadT_Sevt0_5_FSEVT2_7_ISR( void )
{
volatile Uint32 intFlag = IntcRegs->MEVTFLAG[3];
while(intFlag)
{
IntcRegs->EVTCLR[3] = intFlag;
AIF_fsyncEvent2_7Count
(
intFlag
);
//make sure all pending events are handled before return
intFlag = IntcRegs->MEVTFLAG[3];
}
}
In my understanding of SYS/Bios I do not care about the Mask Event Flag(MEVTFLAG)/ Event Clear(EVTCLR) Register, because SYS/Bios will handle that for me via the Hardware Abstraction Layer. Is this assumption correct?
Thanking you in anticipation,
Sebastian