This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HDMI output for OMAP4460 Blaze

Hi,

I have the problem about the image which output from HDMI interface.
The image always get blurred when output from HDMI interface with the resolution = 1920x1080.

The reason why the image get blurred I think the reason might be
"The same input image from the pipeline for both DSI and HDMI video encoder.
It uses the mirror method to duplicate and expand the image as the input image
for the video encoder."

Is that correct ?

Here is the log message from hwc:

D/ti_hwc  (  110): set
H{0x13d0308:DSS,960*800(ARGB32) 0x13cc4e8:DSS,480*800(ARGB32) 0x13d2138:DSS,480*38(RGB565)}
D{0=00000000:960*800,xRGB32 1=00000001:480*800,ARGB32 2=00000002:480*38,RGB565}
L{0x13d0308 0x13cc4e8 0x13d2138}

Could you please help us to figure out how to solve this problem ?

Any suggestion will be appreciated.

Nicholas