Hello All
We have integrated our MPEG2 Encoder with OMX framework on DM8168 netra processor...When we run mpeg2 first time it works fine for any number of frames or any number if hours...But when we run it second time we observed when we call HDVICP Acquire API the app is getting crashed...
Please let us know what could be the problem..Appreciate your help in this regard
.The follwoing is the log error...
Ducati 000 STMXport_printf(...) Depreciated API: TRACE: Nothing to do
Ducati 000 STMXport_printf(...) Depreciated API: TRACE: Nothing to do
[t=0x00000013:398db8a3] ti.sysbios.family.arm.m3.Hwi: ERROR: line 818: E_hardFault: FORCED ti.sysbios.family.arm.m3.Hwi: line 818: E_hardFault: FORCED [t=0x00000013:39908031] ti.sysbios.family.arm.m3.Hwi: ERROR: line 863: E_memFault: IACCVIOL ti.sysbios.family.arm.m3.Hwi: line 863: E_memFault: IACCVIOL Exception occurred in background thread. Exception occurred in ThreadType_Task. Task handle: 0x9971d428. Task stack base: 0x9acda260. Task stack size: 0x4000. R0 = 0x9974a700 R8 = 0xdeadbeef R1 = 0x99d8c2c0 R9 = 0x9acd5aa8 R2 = 0xe014f800 R10 = 0x9ac1e0cc R3 = 0x9e37e725 R11 = 0x9acde04c R4 = 0x00000090 R12 = 0x9e348cac R5 = 0x9aa1afac SP(R13) = 0x9acddf58 R6 = 0x00000004 LR(R14) = 0x9e348b6f R7 = 0x99d8c328 PC(R15) = 0xe014f800 PSR = 0x80000000 ICSR = 0x0440f803 MMFSR = 0x01 BFSR = 0x00 UFSR = 0x0000 HFSR = 0x40000000 DFSR = 0x00000000 MMAR = 0xe000ed34 BFAR = 0xe000ed38 AFSR = 0x00000000 Terminating execution...