Other Parts Discussed in Thread: TMS320C6671
I am testing my code for MSI interrupts using a TMS320C6678EVM board operating as an RC running CCS 5.1.0. I have no EP, but think I should be able to trigger the MSI interrupts to verify my code without one. I am triggering the MSI interrupts both by writing to the MSI IRQ register in directly or writing to the appropriate raw register using Memory Browser. I have enabled several interrupts on all 8 enable registers and can see they are enabled using the memory browser on the that memory (starting at 0x21800054). When I trigger 0, 8, 16 or 24 (all in MSI0), the ISR gets called, any other single interrupt, and the ISR does not get called, even though the interrupts are enabled.