This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Using XDAIS on C6713



Hello.

I would like to transform my algorithm to xdm package. I use CCS v5.1.0.201104171800 with xdais 7.23.0.06. and i have a few questions.

1. Does C6713 supported by XDAIS ?
When i run XDM GenAlg wizard, C6713 is not in the list of availible targets.

2. What type of "Base Interface" i should choose? I want develop a echo canceler, so i need two input signals and one output signal, nothing more.

  • lexa fedotov said:
    1. Does C6713 supported by XDAIS ?
    When i run XDM GenAlg wizard, C6713 is not in the list of availible targets.

    XDAIS itself is not processor-dependent, but some of the GUIs and other tooling only support more recent cores like 64x+ and 674x.  I think you're going to have an uphill battle trying to use c6713.  That device is around 10 years old now so I highly recommend updating to something newer such as c6748. 

    lexa fedotov said:
    2. What type of "Base Interface" i should choose? I want develop a echo canceler, so i need two input signals and one output signal, nothing more.

    I recommend moving to c6748 and using IUNIVERSAL interface as described here:

    http://processors.wiki.ti.com/index.php/Getting_started_with_IUNIVERSAL