Other Parts Discussed in Thread: TMS320C5535
Hello,
i use the TMS320C5535 eZdsp USB evaluation board and have some problems with the UART.
I need the GPIO Pins (actually two Led's) for time measurement. Anymore i want to use the UART to send results (computed results with the FFT-Function) to the Hyperterminal. One of the functions run, the GPIO without the UART and the UART without the GPIO. If i want to use booth functions in my code, the program hang. In any case i use the CSL Framework.
So my question is, if i can configurate the UART and GPIO without the Framework, because i think that the Frameworks are not compatible? But i didn't find any code or help in the Datasheets to use the GPIO or UART and the other peripherie (e.g. Timer) without the CSL Framework.
Edit: I start another try and step through my code. After the GPIO initialisation i write a "1" to my LEDs and they turn off. Some lines after that, i start the UART initialisation and it seems like the registers are overwriten. The LEDs turn on, and the program hang by the UART_config instruction one line later.