Question from customer:
We have a question regarding the Audio Capacitive Touch BoosterPack Hardware from TI, including the C5535 DSP.
Here, it say:
http://processors.wiki.ti.com/index.php/Audio_Capacitive_Touch_BoosterPack_Hardware#Q:_Can_I_connect_a_JTAG_debugger_to_P1:JTAG_Interface.3F
Q: Can I connect a JTAG debugger to P1:JTAG Interface?
A: No. To protect licensed MP3 encode and decode source code the JTAG of the C5535 DSP on each ACTBP is disabled
- So, if the JTAG is disabled, how can we program the C5535?
- Is there a way to use custom code on the C5535 of this Booster pack?
Thanks and best regards,
Anthony