This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

D1 resolution on IPNC_DM812X_2.0.0

Hi,

   I'm using IPNC 2.0.0 multich_tristream usecase.  I try to change the second stream(D1) to PAL mode by making some changes in the project:

   1.multich_tristream_fulfeature.c : change 480 -> 576, the param will be sent to captureLink to creat camera instance

   2. iss_drv_captureApi.c :in which I change some configuration of resizor B

   3. some changes in streamSysInit maybe.

   The result I changed seems no working at all.I changed back 576 ->480 and then it works well.So I suppose there may be somewhere I ignored to apply the D1    resolution changes.  Will anyone please give me some suggestions?

Thanks!