Hello.
I am referencing advisory 2.1.4 on errata (sprz314e).
It describes that Vil driven need to be driven below 0.4V when Dual-Voltage LVCMOS operated at 3.3V.
Although I think it will be applied when only operated at 3.3V,
the description of datasheet(sprs658d) specifies that Vil is about 0.63V(0.35 x DVDD) on 1.8V operation.
Since it is higher than 0.4V, I worry it .
This issue is NOT applied when the Dual-Voltage LVCMOS operated at 1.8V.
Is it correct?
Best regards,
RY