How do I obtain and install correct eZdsp5535 drivers in place of original microsoft USB drivers? When checking device manager with eZdsp5535 connected I see no TI drivers, just original microsoft PC USB drivers. I also use 28027 piccolo stick and when I connect it to USB the two TI driver channels correctly appear in the device manager so this can happen but 5535 USB connection shows no Ti driver channels for 5535. Reconnecting 5535 does not fix this. Where can the drivers be found and how do they install? Should they have auto-installed with CCS5.2? Other CCS5.2 settings apparently correct for eZdsp5535. Using the PC resource for changing drivers only reinstalls the original Microsoft PC drivers.
Larry