This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM648 QDMA



Hello everyone:

      I have a problem in use QDMA in  CCS3.3 DM648 board.   I am using the QDMA by directly writing into the QDMA registers.  I spent a long time to get it going , but it still have some problem.  I just  want to copy data from  external memory  to L2.  It can copy some data ,but not all data.  Then I use EDMA in DVSDK , it has the same problem.

But when I use memcpy , it is ok.

What is the problem?

My code:

#define  PARAM_ENTRY_USED   80
#define  TCC_USE            0
S32 DAT_Open(U32 chaNum)
{
    volatile U32 *p_QDMA_CHMAP0 = (volatile U32 *)(QDMA_CHMAP0_ADDR);

    if(chaNum > 7)
    {
        return -1;
    }


    *(volatile U32 *)(QDMA_QRAE0_ADDR)  = 0x000000ff;
   
    //Setting QDMA CHMAP: Parameter entry and trigger word
    p_QDMA_CHMAP0[chaNum] = ((PARAM_ENTRY_USED+chaNum)<<5) + 12;

    //enable the channel in QEER (QDMA Event Enable Register)
    *(volatile U32 *)(QDMA_QEESR_ADDR)  = 0x000000ff;

    return chaNum;
}
void DAT_copy(void *src , void *dst , U16 byteCnt, U16 chaNum)
{

    volatile S32 * base;

    base = (volatile S32 *)(QDMA_PARAM80_ADDR + chaNum*32);

    base[0] = 0x00100008 + ((TCC_USE + chaNum)<<12);
    base[1] = (S32)src;
    base[2] = 0x00010000 + byteCnt;
    base[4] = 0;
    base[5] = 0x0000ffff;
    base[6] = 0;
    base[7] = 1;
    base[3] = (S32)dst;
}
 void DAT_Copy_2D(void *src , void *dst , U16 lineLen, U16 lineCnt, U16 srcPitch, U16 dstPitch, U16 chaNum)
{

    volatile U32 * base;
    base = (volatile U32 *)(QDMA_PARAM80_ADDR + chaNum*32);

    base[0] = 0x0010000c + ((TCC_USE + chaNum)<<12);
    base[1] = (U32)src;
    base[2] = ((U32)lineCnt<<16) + lineLen;
    base[4] = ((U32)dstPitch<<16) + srcPitch;
    base[5] = 0x0000ffff;
    base[6] = 0;
    base[7] = 1;
    base[3] = (U32)dst;
}
void DAT_Wait_6446(U32 id)
{
    volatile U32 * ptr_ipr ;
    volatile U32 * ptr_iprh ;
    volatile U32 * ptr_icr ;
    volatile U32 * ptr_icrh ;

    ptr_ipr = (volatile U32 *)(IPR_ADDR);
    ptr_iprh = (volatile U32 *)(IPRH_ADDR);
    ptr_icr = (volatile U32 *)(ICR_ADDR);
    ptr_icrh = (volatile U32 *)(ICRH_ADDR);

    if((id+TCC_USE)<32)
    {
        while (!(ptr_ipr[0]&(1<<(id + TCC_USE)))) ; //wait for the dma transfer specified by id completing
        ptr_icr[0] |= 1<<(id + TCC_USE);            //clear the setted bit in ipr register
    }
    else
    {
        while (!(ptr_iprh[0]&(1<<(id+TCC_USE-32)))) ;
        ptr_icrh[0] |= 1<<(id+TCC_USE-32);
    }
}