This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Help for the DM365/DM368 USB gadget kernel module could not be insmod

Other Parts Discussed in Thread: DAC7512, ADS7846, TSC2007, TSC2004, PCF8574, LM63, LM70, LM73, LM77, LM80, LM83, LM87, LM90, LM92, LM93, LM95241, ADS7828, ADS7871, AMC6821, TMP102, TMP401, TMP421, TPS65010, TLV320AIC23B, TVP5150, TVP7002, THS7303, THS7353, DA8XX, LP3944, LP5521, LP5523, DAC124S085

I enabled USB webcam gadget kernel module as below config told:

diff psp/linux-2.6.37-psp03.22.00.01/.config.org psp/linux-2.6.37-psp03.22.00.01/.config
4c4
< # Sat Aug 25 11:04:54 2012
---
> # Sat Aug 25 16:23:31 2012
1341c1341,1395
< # CONFIG_V4L_USB_DRIVERS is not set
---
> CONFIG_V4L_USB_DRIVERS=y
> CONFIG_USB_VIDEO_CLASS=y
> CONFIG_USB_VIDEO_CLASS_INPUT_EVDEV=y
> CONFIG_USB_GSPCA=m
> # CONFIG_USB_M5602 is not set
> # CONFIG_USB_STV06XX is not set
> # CONFIG_USB_GL860 is not set
> # CONFIG_USB_GSPCA_BENQ is not set
> # CONFIG_USB_GSPCA_CONEX is not set
> # CONFIG_USB_GSPCA_CPIA1 is not set
> # CONFIG_USB_GSPCA_ETOMS is not set
> # CONFIG_USB_GSPCA_FINEPIX is not set
> # CONFIG_USB_GSPCA_JEILINJ is not set
> # CONFIG_USB_GSPCA_KONICA is not set
> # CONFIG_USB_GSPCA_MARS is not set
> # CONFIG_USB_GSPCA_MR97310A is not set
> # CONFIG_USB_GSPCA_OV519 is not set
> # CONFIG_USB_GSPCA_OV534 is not set
> # CONFIG_USB_GSPCA_OV534_9 is not set
> # CONFIG_USB_GSPCA_PAC207 is not set
> # CONFIG_USB_GSPCA_PAC7302 is not set
> # CONFIG_USB_GSPCA_PAC7311 is not set
> # CONFIG_USB_GSPCA_SN9C2028 is not set
> # CONFIG_USB_GSPCA_SN9C20X is not set
> # CONFIG_USB_GSPCA_SONIXB is not set
> # CONFIG_USB_GSPCA_SONIXJ is not set
> # CONFIG_USB_GSPCA_SPCA500 is not set
> # CONFIG_USB_GSPCA_SPCA501 is not set
> # CONFIG_USB_GSPCA_SPCA505 is not set
> # CONFIG_USB_GSPCA_SPCA506 is not set
> # CONFIG_USB_GSPCA_SPCA508 is not set
> # CONFIG_USB_GSPCA_SPCA561 is not set
> # CONFIG_USB_GSPCA_SPCA1528 is not set
> # CONFIG_USB_GSPCA_SQ905 is not set
> # CONFIG_USB_GSPCA_SQ905C is not set
> # CONFIG_USB_GSPCA_SQ930X is not set
> # CONFIG_USB_GSPCA_STK014 is not set
> # CONFIG_USB_GSPCA_STV0680 is not set
> # CONFIG_USB_GSPCA_SUNPLUS is not set
> # CONFIG_USB_GSPCA_T613 is not set
> # CONFIG_USB_GSPCA_TV8532 is not set
> # CONFIG_USB_GSPCA_VC032X is not set
> # CONFIG_USB_GSPCA_XIRLINK_CIT is not set
> # CONFIG_USB_GSPCA_ZC3XX is not set
> # CONFIG_VIDEO_PVRUSB2 is not set
> # CONFIG_VIDEO_HDPVR is not set
> # CONFIG_VIDEO_EM28XX is not set
> # CONFIG_VIDEO_CX231XX is not set
> # CONFIG_VIDEO_USBVISION is not set
> # CONFIG_USB_ET61X251 is not set
> # CONFIG_USB_SN9C102 is not set
> # CONFIG_USB_PWC is not set
> # CONFIG_USB_ZR364XX is not set
> # CONFIG_USB_STKWEBCAM is not set
> # CONFIG_USB_S2255 is not set
1544a1599
> # CONFIG_USB_MUSB_PERIPHERAL is not set
1621c1676,1701
< # CONFIG_USB_GADGET is not set
---
> CONFIG_USB_GADGET=y
> # CONFIG_USB_GADGET_DEBUG is not set
> # CONFIG_USB_GADGET_DEBUG_FILES is not set
> # CONFIG_USB_GADGET_DEBUG_FS is not set
> CONFIG_USB_GADGET_VBUS_DRAW=2
> CONFIG_USB_GADGET_SELECTED=y
> CONFIG_USB_GADGET_R8A66597=y
> CONFIG_USB_R8A66597=y
> # CONFIG_USB_GADGET_M66592 is not set
> # CONFIG_USB_GADGET_DUMMY_HCD is not set
> CONFIG_USB_GADGET_DUALSPEED=y
> # CONFIG_USB_ZERO is not set
> # CONFIG_USB_AUDIO is not set
> # CONFIG_USB_ETH is not set
> # CONFIG_USB_GADGETFS is not set
> # CONFIG_USB_FUNCTIONFS is not set
> # CONFIG_USB_FILE_STORAGE is not set
> # CONFIG_USB_MASS_STORAGE is not set
> # CONFIG_USB_G_SERIAL is not set
> # CONFIG_USB_MIDI_GADGET is not set
> # CONFIG_USB_G_PRINTER is not set
> # CONFIG_USB_CDC_COMPOSITE is not set
> # CONFIG_USB_G_MULTI is not set
> # CONFIG_USB_G_HID is not set
> # CONFIG_USB_G_DBGP is not set
> CONFIG_USB_G_WEBCAM=m

When i try to insmod g_webcam.ko, it told error like below:

root@dm368-evm:~# modprobe g_webcam
FATAL: Error inserting g_webcam (/lib/modules/2.6.37/kernel/drivers/usb/gadget/g_webcam.ko): No such device

  • The obvious question...does "/lib/modules/2.6.37/kernel/drivers/usb/gadget/g_webcam.ko" exist?

    Maybe try insmod instead of modprobe. The modprobe utility relies on a dependencies file. If you want to use modprobe, you might have to "depmod -a" to update the dependency file after you updated the "/lib/modules" directory.

  • It seems like the kernel, which is running, is not the one which is built along with the g_webcam.ko. The running kernel already has g_webcam built in.

  • Hi Norman,

    tried your suggestion, same error:

    ---------------------------------------------------------------------

    root@dm368-evm:/lib/modules/2.6.37/kernel/drivers/usb/gadget#
    root@dm368-evm:/lib/modules/2.6.37/kernel/drivers/usb/gadget# ls
    g_webcam.ko
    root@dm368-evm:/lib/modules/2.6.37/kernel/drivers/usb/gadget# insmod g_webcam.ko


    insmod: error inserting 'g_webcam.ko': -1 No such device

    -----------------------------------------------------------------------

  • try 'zcat /proc/config.gz | grep CONFIG_USB_G_WEBCAM' to see what it tells.

  • Hi Bin,

    Thanks for your suggestion.

    I find the root cause after i try "make menuconfig" for another kernel configuration.

    The right kernel config should (based on original davinci_dm365_defconfig):

    1. Enable

    Device Drivers -> Multimedia support -> Video capture adapter -> V4L USB devices -> USB video class (UVC)

    (not sure it is must one or not ) Device Drivers -> Multimedia support -> Video capture adapter -> V4L USB devices -> UVC input event devices support

    2. Disable(maybe we can support OTG with host together, but i disabled it)

    Device Drivers -> USB support -> Support for Host side USB  [disable it]

    3. Enable

    Device Drivers -> USB support -> USB gadget support  -> USB Peripheral Controller -> Inventra HDRC USB Peripheral (TI, ADI, ....)

    4. Enable (M)

    Device Drivers -> USB support -> USB gadget support  -> USB Gadget Drivers -> USB Webam Gadget

    BTW: after steps 1 ~ 4, step 1 could not be seen any more, I do not study why.

    I copy my .config here:

    ----------------------------------------------------------------------------------------------------------------------------

    #
    # Automatically generated make config: don't edit
    # Linux/arm 2.6.37 Kernel Configuration
    # Tue Aug 28 23:27:14 2012
    #
    CONFIG_ARM=y
    CONFIG_SYS_SUPPORTS_APM_EMULATION=y
    CONFIG_GENERIC_GPIO=y
    # CONFIG_ARCH_USES_GETTIMEOFFSET is not set
    CONFIG_GENERIC_CLOCKEVENTS=y
    CONFIG_HAVE_PROC_CPU=y
    CONFIG_GENERIC_HARDIRQS=y
    CONFIG_STACKTRACE_SUPPORT=y
    CONFIG_HAVE_LATENCYTOP_SUPPORT=y
    CONFIG_LOCKDEP_SUPPORT=y
    CONFIG_TRACE_IRQFLAGS_SUPPORT=y
    CONFIG_HARDIRQS_SW_RESEND=y
    CONFIG_GENERIC_IRQ_PROBE=y
    CONFIG_RWSEM_GENERIC_SPINLOCK=y
    CONFIG_ARCH_HAS_CPU_IDLE_WAIT=y
    CONFIG_GENERIC_HWEIGHT=y
    CONFIG_GENERIC_CALIBRATE_DELAY=y
    CONFIG_ZONE_DMA=y
    CONFIG_NEED_DMA_MAP_STATE=y
    CONFIG_GENERIC_HARDIRQS_NO__DO_IRQ=y
    CONFIG_VECTORS_BASE=0xffff0000
    CONFIG_DEFCONFIG_LIST="/lib/modules/$UNAME_RELEASE/.config"
    CONFIG_CONSTRUCTORS=y
    CONFIG_HAVE_IRQ_WORK=y

    #
    # General setup
    #
    CONFIG_EXPERIMENTAL=y
    CONFIG_BROKEN_ON_SMP=y
    CONFIG_LOCK_KERNEL=y
    CONFIG_INIT_ENV_ARG_LIMIT=32
    CONFIG_CROSS_COMPILE=""
    CONFIG_LOCALVERSION=""
    # CONFIG_LOCALVERSION_AUTO is not set
    CONFIG_HAVE_KERNEL_GZIP=y
    CONFIG_HAVE_KERNEL_LZMA=y
    CONFIG_HAVE_KERNEL_LZO=y
    CONFIG_KERNEL_GZIP=y
    # CONFIG_KERNEL_LZMA is not set
    # CONFIG_KERNEL_LZO is not set
    # CONFIG_SWAP is not set
    CONFIG_SYSVIPC=y
    CONFIG_SYSVIPC_SYSCTL=y
    CONFIG_POSIX_MQUEUE=y
    CONFIG_POSIX_MQUEUE_SYSCTL=y
    # CONFIG_BSD_PROCESS_ACCT is not set
    # CONFIG_TASKSTATS is not set
    # CONFIG_AUDIT is not set
    # CONFIG_HAVE_GENERIC_HARDIRQS is not set
    # CONFIG_SPARSE_IRQ is not set

    #
    # RCU Subsystem
    #
    CONFIG_TREE_PREEMPT_RCU=y
    # CONFIG_TINY_RCU is not set
    # CONFIG_TINY_PREEMPT_RCU is not set
    CONFIG_PREEMPT_RCU=y
    # CONFIG_RCU_TRACE is not set
    CONFIG_RCU_FANOUT=32
    # CONFIG_RCU_FANOUT_EXACT is not set
    # CONFIG_TREE_RCU_TRACE is not set
    CONFIG_IKCONFIG=y
    CONFIG_IKCONFIG_PROC=y
    CONFIG_LOG_BUF_SHIFT=14
    # CONFIG_CGROUPS is not set
    # CONFIG_NAMESPACES is not set
    # CONFIG_SYSFS_DEPRECATED is not set
    # CONFIG_RELAY is not set
    CONFIG_BLK_DEV_INITRD=y
    CONFIG_INITRAMFS_SOURCE=""
    CONFIG_RD_GZIP=y
    # CONFIG_RD_BZIP2 is not set
    # CONFIG_RD_LZMA is not set
    # CONFIG_RD_LZO is not set
    CONFIG_CC_OPTIMIZE_FOR_SIZE=y
    CONFIG_SYSCTL=y
    CONFIG_ANON_INODES=y
    CONFIG_EMBEDDED=y
    CONFIG_UID16=y
    CONFIG_SYSCTL_SYSCALL=y
    CONFIG_KALLSYMS=y
    # CONFIG_KALLSYMS_ALL is not set
    # CONFIG_KALLSYMS_EXTRA_PASS is not set
    CONFIG_HOTPLUG=y
    CONFIG_PRINTK=y
    CONFIG_BUG=y
    CONFIG_ELF_CORE=y
    CONFIG_BASE_FULL=y
    CONFIG_FUTEX=y
    CONFIG_EPOLL=y
    CONFIG_SIGNALFD=y
    CONFIG_TIMERFD=y
    CONFIG_EVENTFD=y
    CONFIG_SHMEM=y
    CONFIG_AIO=y
    CONFIG_HAVE_PERF_EVENTS=y
    CONFIG_PERF_USE_VMALLOC=y

    #
    # Kernel Performance Events And Counters
    #
    # CONFIG_PERF_EVENTS is not set
    # CONFIG_PERF_COUNTERS is not set
    CONFIG_VM_EVENT_COUNTERS=y
    CONFIG_SLUB_DEBUG=y
    CONFIG_COMPAT_BRK=y
    # CONFIG_SLAB is not set
    CONFIG_SLUB=y
    # CONFIG_SLOB is not set
    # CONFIG_PROFILING is not set
    CONFIG_HAVE_OPROFILE=y
    # CONFIG_KPROBES is not set
    CONFIG_HAVE_KPROBES=y
    CONFIG_HAVE_KRETPROBES=y
    CONFIG_HAVE_REGS_AND_STACK_ACCESS_API=y
    CONFIG_HAVE_CLK=y

    #
    # GCOV-based kernel profiling
    #
    # CONFIG_GCOV_KERNEL is not set
    CONFIG_HAVE_GENERIC_DMA_COHERENT=y
    CONFIG_SLABINFO=y
    CONFIG_RT_MUTEXES=y
    CONFIG_BASE_SMALL=0
    CONFIG_MODULES=y
    # CONFIG_MODULE_FORCE_LOAD is not set
    CONFIG_MODULE_UNLOAD=y
    CONFIG_MODULE_FORCE_UNLOAD=y
    CONFIG_MODVERSIONS=y
    # CONFIG_MODULE_SRCVERSION_ALL is not set
    CONFIG_BLOCK=y
    CONFIG_LBDAF=y
    # CONFIG_BLK_DEV_BSG is not set
    # CONFIG_BLK_DEV_INTEGRITY is not set

    #
    # IO Schedulers
    #
    CONFIG_IOSCHED_NOOP=y
    # CONFIG_IOSCHED_DEADLINE is not set
    # CONFIG_IOSCHED_CFQ is not set
    CONFIG_DEFAULT_NOOP=y
    CONFIG_DEFAULT_IOSCHED="noop"
    # CONFIG_INLINE_SPIN_TRYLOCK is not set
    # CONFIG_INLINE_SPIN_TRYLOCK_BH is not set
    # CONFIG_INLINE_SPIN_LOCK is not set
    # CONFIG_INLINE_SPIN_LOCK_BH is not set
    # CONFIG_INLINE_SPIN_LOCK_IRQ is not set
    # CONFIG_INLINE_SPIN_LOCK_IRQSAVE is not set
    # CONFIG_INLINE_SPIN_UNLOCK is not set
    # CONFIG_INLINE_SPIN_UNLOCK_BH is not set
    # CONFIG_INLINE_SPIN_UNLOCK_IRQ is not set
    # CONFIG_INLINE_SPIN_UNLOCK_IRQRESTORE is not set
    # CONFIG_INLINE_READ_TRYLOCK is not set
    # CONFIG_INLINE_READ_LOCK is not set
    # CONFIG_INLINE_READ_LOCK_BH is not set
    # CONFIG_INLINE_READ_LOCK_IRQ is not set
    # CONFIG_INLINE_READ_LOCK_IRQSAVE is not set
    # CONFIG_INLINE_READ_UNLOCK is not set
    # CONFIG_INLINE_READ_UNLOCK_BH is not set
    # CONFIG_INLINE_READ_UNLOCK_IRQ is not set
    # CONFIG_INLINE_READ_UNLOCK_IRQRESTORE is not set
    # CONFIG_INLINE_WRITE_TRYLOCK is not set
    # CONFIG_INLINE_WRITE_LOCK is not set
    # CONFIG_INLINE_WRITE_LOCK_BH is not set
    # CONFIG_INLINE_WRITE_LOCK_IRQ is not set
    # CONFIG_INLINE_WRITE_LOCK_IRQSAVE is not set
    # CONFIG_INLINE_WRITE_UNLOCK is not set
    # CONFIG_INLINE_WRITE_UNLOCK_BH is not set
    # CONFIG_INLINE_WRITE_UNLOCK_IRQ is not set
    # CONFIG_INLINE_WRITE_UNLOCK_IRQRESTORE is not set
    # CONFIG_MUTEX_SPIN_ON_OWNER is not set
    # CONFIG_FREEZER is not set

    #
    # System Type
    #
    CONFIG_MMU=y
    # CONFIG_ARCH_AAEC2000 is not set
    # CONFIG_ARCH_INTEGRATOR is not set
    # CONFIG_ARCH_REALVIEW is not set
    # CONFIG_ARCH_VERSATILE is not set
    # CONFIG_ARCH_VEXPRESS is not set
    # CONFIG_ARCH_AT91 is not set
    # CONFIG_ARCH_BCMRING is not set
    # CONFIG_ARCH_CLPS711X is not set
    # CONFIG_ARCH_CNS3XXX is not set
    # CONFIG_ARCH_GEMINI is not set
    # CONFIG_ARCH_EBSA110 is not set
    # CONFIG_ARCH_EP93XX is not set
    # CONFIG_ARCH_FOOTBRIDGE is not set
    # CONFIG_ARCH_MXC is not set
    # CONFIG_ARCH_STMP3XXX is not set
    # CONFIG_ARCH_NETX is not set
    # CONFIG_ARCH_H720X is not set
    # CONFIG_ARCH_IOP13XX is not set
    # CONFIG_ARCH_IOP32X is not set
    # CONFIG_ARCH_IOP33X is not set
    # CONFIG_ARCH_IXP23XX is not set
    # CONFIG_ARCH_IXP2000 is not set
    # CONFIG_ARCH_IXP4XX is not set
    # CONFIG_ARCH_DOVE is not set
    # CONFIG_ARCH_KIRKWOOD is not set
    # CONFIG_ARCH_LOKI is not set
    # CONFIG_ARCH_LPC32XX is not set
    # CONFIG_ARCH_MV78XX0 is not set
    # CONFIG_ARCH_ORION5X is not set
    # CONFIG_ARCH_MMP is not set
    # CONFIG_ARCH_KS8695 is not set
    # CONFIG_ARCH_NS9XXX is not set
    # CONFIG_ARCH_W90X900 is not set
    # CONFIG_ARCH_NUC93X is not set
    # CONFIG_ARCH_TEGRA is not set
    # CONFIG_ARCH_PNX4008 is not set
    # CONFIG_ARCH_PXA is not set
    # CONFIG_ARCH_MSM is not set
    # CONFIG_ARCH_SHMOBILE is not set
    # CONFIG_ARCH_RPC is not set
    # CONFIG_ARCH_SA1100 is not set
    # CONFIG_ARCH_S3C2410 is not set
    # CONFIG_ARCH_S3C64XX is not set
    # CONFIG_ARCH_S5P64X0 is not set
    # CONFIG_ARCH_S5P6442 is not set
    # CONFIG_ARCH_S5PC100 is not set
    # CONFIG_ARCH_S5PV210 is not set
    # CONFIG_ARCH_S5PV310 is not set
    # CONFIG_ARCH_SHARK is not set
    # CONFIG_ARCH_TCC_926 is not set
    # CONFIG_ARCH_LH7A40X is not set
    # CONFIG_ARCH_U300 is not set
    # CONFIG_ARCH_U8500 is not set
    # CONFIG_ARCH_NOMADIK is not set
    CONFIG_ARCH_DAVINCI=y
    # CONFIG_ARCH_OMAP is not set
    # CONFIG_PLAT_SPEAR is not set
    CONFIG_AINTC=y
    CONFIG_ARCH_DAVINCI_DMx=y

    #
    # TI DaVinci Implementations
    #

    #
    # DaVinci Core Type
    #
    # CONFIG_ARCH_DAVINCI_DM644x is not set
    # CONFIG_ARCH_DAVINCI_DM355 is not set
    # CONFIG_ARCH_DAVINCI_DM646x is not set
    # CONFIG_ARCH_DAVINCI_DA830 is not set
    # CONFIG_ARCH_DAVINCI_DA850 is not set
    CONFIG_ARCH_DAVINCI_DM365=y
    # CONFIG_ARCH_DAVINCI_TNETV107X is not set

    #
    # DaVinci Board Type
    #
    CONFIG_MACH_DAVINCI_DM365_EVM=y
    # CONFIG_GPIO_PCA953X is not set
    # CONFIG_KEYBOARD_GPIO_POLLED is not set
    CONFIG_DAVINCI_MUX=y
    # CONFIG_DAVINCI_MUX_DEBUG is not set
    # CONFIG_DAVINCI_MUX_WARNINGS is not set
    CONFIG_DAVINCI_RESET_CLOCKS=y
    # CONFIG_DAVINCI_MCBSP is not set

    #
    # Processor Type
    #
    CONFIG_CPU_ARM926T=y
    CONFIG_CPU_32v5=y
    CONFIG_CPU_ABRT_EV5TJ=y
    CONFIG_CPU_PABRT_LEGACY=y
    CONFIG_CPU_CACHE_VIVT=y
    CONFIG_CPU_COPY_V4WB=y
    CONFIG_CPU_TLB_V4WBI=y
    CONFIG_CPU_CP15=y
    CONFIG_CPU_CP15_MMU=y

    #
    # Processor Features
    #
    CONFIG_ARM_THUMB=y
    # CONFIG_CPU_ICACHE_DISABLE is not set
    # CONFIG_CPU_DCACHE_DISABLE is not set
    # CONFIG_CPU_DCACHE_WRITETHROUGH is not set
    # CONFIG_CPU_CACHE_ROUND_ROBIN is not set
    CONFIG_ARM_L1_CACHE_SHIFT=5
    CONFIG_COMMON_CLKDEV=y

    #
    # Bus support
    #
    # CONFIG_PCI_SYSCALL is not set
    # CONFIG_ARCH_SUPPORTS_MSI is not set
    # CONFIG_PCCARD is not set

    #
    # Kernel Features
    #
    CONFIG_TICK_ONESHOT=y
    CONFIG_NO_HZ=y
    CONFIG_HIGH_RES_TIMERS=y
    CONFIG_GENERIC_CLOCKEVENTS_BUILD=y
    CONFIG_VMSPLIT_3G=y
    # CONFIG_VMSPLIT_2G is not set
    # CONFIG_VMSPLIT_1G is not set
    CONFIG_PAGE_OFFSET=0xC0000000
    # CONFIG_PREEMPT_NONE is not set
    # CONFIG_PREEMPT_VOLUNTARY is not set
    CONFIG_PREEMPT=y
    CONFIG_HZ=100
    CONFIG_AEABI=y
    # CONFIG_OABI_COMPAT is not set
    CONFIG_ARCH_HAS_HOLES_MEMORYMODEL=y
    # CONFIG_ARCH_SPARSEMEM_DEFAULT is not set
    # CONFIG_ARCH_SELECT_MEMORY_MODEL is not set
    # CONFIG_HIGHMEM is not set
    CONFIG_SELECT_MEMORY_MODEL=y
    CONFIG_FLATMEM_MANUAL=y
    CONFIG_FLATMEM=y
    CONFIG_FLAT_NODE_MEM_MAP=y
    CONFIG_HAVE_MEMBLOCK=y
    CONFIG_PAGEFLAGS_EXTENDED=y
    CONFIG_SPLIT_PTLOCK_CPUS=999999
    # CONFIG_PHYS_ADDR_T_64BIT is not set
    CONFIG_ZONE_DMA_FLAG=1
    CONFIG_BOUNCE=y
    CONFIG_VIRT_TO_BUS=y
    # CONFIG_KSM is not set
    CONFIG_DEFAULT_MMAP_MIN_ADDR=4096
    CONFIG_NEED_PER_CPU_KM=y
    CONFIG_FORCE_MAX_ZONEORDER=11
    CONFIG_LEDS=y
    # CONFIG_LEDS_CPU is not set
    CONFIG_ALIGNMENT_TRAP=y
    # CONFIG_UACCESS_WITH_MEMCPY is not set
    # CONFIG_SECCOMP is not set
    # CONFIG_CC_STACKPROTECTOR is not set
    # CONFIG_DEPRECATED_PARAM_STRUCT is not set

    #
    # Boot options
    #
    CONFIG_ZBOOT_ROM_TEXT=0x0
    CONFIG_ZBOOT_ROM_BSS=0x0
    CONFIG_CMDLINE=""
    # CONFIG_XIP_KERNEL is not set
    # CONFIG_KEXEC is not set
    # CONFIG_AUTO_ZRELADDR is not set

    #
    # CPU Power Management
    #
    # CONFIG_CPU_IDLE is not set

    #
    # Floating point emulation
    #

    #
    # At least one emulation must be selected
    #
    # CONFIG_VFP is not set

    #
    # Userspace binary formats
    #
    CONFIG_BINFMT_ELF=y
    # CONFIG_CORE_DUMP_DEFAULT_ELF_HEADERS is not set
    CONFIG_HAVE_AOUT=y
    # CONFIG_BINFMT_AOUT is not set
    # CONFIG_BINFMT_MISC is not set

    #
    # Power management options
    #
    # CONFIG_PM is not set
    CONFIG_ARCH_SUSPEND_POSSIBLE=y
    CONFIG_NET=y

    #
    # Networking options
    #
    CONFIG_PACKET=y
    CONFIG_UNIX=y
    CONFIG_XFRM=y
    # CONFIG_XFRM_USER is not set
    # CONFIG_XFRM_SUB_POLICY is not set
    # CONFIG_XFRM_MIGRATE is not set
    # CONFIG_XFRM_STATISTICS is not set
    # CONFIG_NET_KEY is not set
    CONFIG_INET=y
    # CONFIG_IP_MULTICAST is not set
    # CONFIG_IP_ADVANCED_ROUTER is not set
    CONFIG_IP_FIB_HASH=y
    CONFIG_IP_PNP=y
    CONFIG_IP_PNP_DHCP=y
    # CONFIG_IP_PNP_BOOTP is not set
    # CONFIG_IP_PNP_RARP is not set
    # CONFIG_NET_IPIP is not set
    # CONFIG_NET_IPGRE_DEMUX is not set
    # CONFIG_ARPD is not set
    # CONFIG_SYN_COOKIES is not set
    # CONFIG_INET_AH is not set
    # CONFIG_INET_ESP is not set
    # CONFIG_INET_IPCOMP is not set
    # CONFIG_INET_XFRM_TUNNEL is not set
    CONFIG_INET_TUNNEL=m
    CONFIG_INET_XFRM_MODE_TRANSPORT=y
    CONFIG_INET_XFRM_MODE_TUNNEL=y
    CONFIG_INET_XFRM_MODE_BEET=y
    # CONFIG_INET_LRO is not set
    CONFIG_INET_DIAG=y
    CONFIG_INET_TCP_DIAG=y
    # CONFIG_TCP_CONG_ADVANCED is not set
    CONFIG_TCP_CONG_CUBIC=y
    CONFIG_DEFAULT_TCP_CONG="cubic"
    # CONFIG_TCP_MD5SIG is not set
    CONFIG_IPV6=m
    # CONFIG_IPV6_PRIVACY is not set
    # CONFIG_IPV6_ROUTER_PREF is not set
    # CONFIG_IPV6_OPTIMISTIC_DAD is not set
    # CONFIG_INET6_AH is not set
    # CONFIG_INET6_ESP is not set
    # CONFIG_INET6_IPCOMP is not set
    # CONFIG_IPV6_MIP6 is not set
    # CONFIG_INET6_XFRM_TUNNEL is not set
    # CONFIG_INET6_TUNNEL is not set
    CONFIG_INET6_XFRM_MODE_TRANSPORT=m
    CONFIG_INET6_XFRM_MODE_TUNNEL=m
    CONFIG_INET6_XFRM_MODE_BEET=m
    # CONFIG_INET6_XFRM_MODE_ROUTEOPTIMIZATION is not set
    CONFIG_IPV6_SIT=m
    # CONFIG_IPV6_SIT_6RD is not set
    CONFIG_IPV6_NDISC_NODETYPE=y
    # CONFIG_IPV6_TUNNEL is not set
    # CONFIG_IPV6_MULTIPLE_TABLES is not set
    # CONFIG_IPV6_MROUTE is not set
    # CONFIG_NETWORK_SECMARK is not set
    # CONFIG_NETWORK_PHY_TIMESTAMPING is not set
    CONFIG_NETFILTER=y
    # CONFIG_NETFILTER_DEBUG is not set
    CONFIG_NETFILTER_ADVANCED=y

    #
    # Core Netfilter Configuration
    #
    # CONFIG_NETFILTER_NETLINK_QUEUE is not set
    # CONFIG_NETFILTER_NETLINK_LOG is not set
    # CONFIG_NF_CONNTRACK is not set
    # CONFIG_NETFILTER_XTABLES is not set
    # CONFIG_IP_VS is not set

    #
    # IP: Netfilter Configuration
    #
    # CONFIG_NF_DEFRAG_IPV4 is not set
    # CONFIG_IP_NF_QUEUE is not set
    # CONFIG_IP_NF_IPTABLES is not set
    # CONFIG_IP_NF_ARPTABLES is not set

    #
    # IPv6: Netfilter Configuration
    #
    # CONFIG_NF_DEFRAG_IPV6 is not set
    # CONFIG_IP6_NF_QUEUE is not set
    # CONFIG_IP6_NF_IPTABLES is not set
    # CONFIG_IP_DCCP is not set
    # CONFIG_IP_SCTP is not set
    # CONFIG_RDS is not set
    # CONFIG_TIPC is not set
    # CONFIG_ATM is not set
    # CONFIG_L2TP is not set
    # CONFIG_BRIDGE is not set
    # CONFIG_NET_DSA is not set
    # CONFIG_VLAN_8021Q is not set
    # CONFIG_DECNET is not set
    # CONFIG_LLC2 is not set
    # CONFIG_IPX is not set
    # CONFIG_ATALK is not set
    # CONFIG_X25 is not set
    # CONFIG_LAPB is not set
    # CONFIG_ECONET is not set
    # CONFIG_WAN_ROUTER is not set
    # CONFIG_PHONET is not set
    # CONFIG_IEEE802154 is not set
    # CONFIG_NET_SCHED is not set
    # CONFIG_DCB is not set

    #
    # Network testing
    #
    # CONFIG_NET_PKTGEN is not set
    # CONFIG_HAMRADIO is not set
    # CONFIG_CAN is not set
    # CONFIG_IRDA is not set
    # CONFIG_BT is not set
    # CONFIG_AF_RXRPC is not set
    CONFIG_WIRELESS=y
    CONFIG_WIRELESS_EXT=y
    CONFIG_WEXT_CORE=y
    CONFIG_WEXT_PROC=y
    CONFIG_WEXT_SPY=y
    CONFIG_CFG80211=y
    # CONFIG_NL80211_TESTMODE is not set
    # CONFIG_CFG80211_DEVELOPER_WARNINGS is not set
    # CONFIG_CFG80211_REG_DEBUG is not set
    CONFIG_CFG80211_DEFAULT_PS=y
    # CONFIG_CFG80211_DEBUGFS is not set
    # CONFIG_CFG80211_INTERNAL_REGDB is not set
    CONFIG_CFG80211_WEXT=y
    CONFIG_WIRELESS_EXT_SYSFS=y
    CONFIG_LIB80211=y
    # CONFIG_LIB80211_DEBUG is not set
    # CONFIG_MAC80211 is not set

    #
    # Some wireless drivers require a rate control algorithm
    #
    # CONFIG_WIMAX is not set
    # CONFIG_RFKILL is not set
    # CONFIG_NET_9P is not set
    # CONFIG_CAIF is not set
    # CONFIG_CEPH_LIB is not set

    #
    # Device Drivers
    #

    #
    # Generic Driver Options
    #
    CONFIG_UEVENT_HELPER_PATH="/sbin/hotplug"
    # CONFIG_DEVTMPFS is not set
    CONFIG_STANDALONE=y
    CONFIG_PREVENT_FIRMWARE_BUILD=y
    CONFIG_FW_LOADER=y
    CONFIG_FIRMWARE_IN_KERNEL=y
    CONFIG_EXTRA_FIRMWARE=""
    # CONFIG_DEBUG_DRIVER is not set
    # CONFIG_DEBUG_DEVRES is not set
    # CONFIG_SYS_HYPERVISOR is not set
    # CONFIG_CONNECTOR is not set
    CONFIG_MTD=y
    # CONFIG_MTD_DEBUG is not set
    CONFIG_MTD_TESTS=m
    # CONFIG_MTD_CONCAT is not set
    CONFIG_MTD_PARTITIONS=y
    # CONFIG_MTD_REDBOOT_PARTS is not set
    CONFIG_MTD_CMDLINE_PARTS=y
    # CONFIG_MTD_AFS_PARTS is not set
    # CONFIG_MTD_AR7_PARTS is not set

    #
    # User Modules And Translation Layers
    #
    CONFIG_MTD_CHAR=y
    CONFIG_MTD_BLKDEVS=y
    CONFIG_MTD_BLOCK=y
    # CONFIG_FTL is not set
    # CONFIG_NFTL is not set
    # CONFIG_INFTL is not set
    # CONFIG_RFD_FTL is not set
    # CONFIG_SSFDC is not set
    # CONFIG_SM_FTL is not set
    # CONFIG_MTD_OOPS is not set

    #
    # RAM/ROM/Flash chip drivers
    #
    # CONFIG_MTD_CFI is not set
    # CONFIG_MTD_JEDECPROBE is not set
    CONFIG_MTD_MAP_BANK_WIDTH_1=y
    CONFIG_MTD_MAP_BANK_WIDTH_2=y
    CONFIG_MTD_MAP_BANK_WIDTH_4=y
    # CONFIG_MTD_MAP_BANK_WIDTH_8 is not set
    # CONFIG_MTD_MAP_BANK_WIDTH_16 is not set
    # CONFIG_MTD_MAP_BANK_WIDTH_32 is not set
    CONFIG_MTD_CFI_I1=y
    CONFIG_MTD_CFI_I2=y
    # CONFIG_MTD_CFI_I4 is not set
    # CONFIG_MTD_CFI_I8 is not set
    # CONFIG_MTD_RAM is not set
    # CONFIG_MTD_ROM is not set
    # CONFIG_MTD_ABSENT is not set

    #
    # Mapping drivers for chip access
    #
    # CONFIG_MTD_COMPLEX_MAPPINGS is not set
    # CONFIG_MTD_PLATRAM is not set

    #
    # Self-contained MTD device drivers
    #
    # CONFIG_MTD_DATAFLASH is not set
    # CONFIG_MTD_M25P80 is not set
    # CONFIG_MTD_SST25L is not set
    # CONFIG_MTD_SLRAM is not set
    # CONFIG_MTD_PHRAM is not set
    # CONFIG_MTD_MTDRAM is not set
    # CONFIG_MTD_BLOCK2MTD is not set

    #
    # Disk-On-Chip Device Drivers
    #
    # CONFIG_MTD_DOC2000 is not set
    # CONFIG_MTD_DOC2001 is not set
    # CONFIG_MTD_DOC2001PLUS is not set
    CONFIG_MTD_NAND_ECC=y
    # CONFIG_MTD_NAND_ECC_SMC is not set
    CONFIG_MTD_NAND=y
    # CONFIG_MTD_NAND_VERIFY_WRITE is not set
    # CONFIG_MTD_SM_COMMON is not set
    # CONFIG_MTD_NAND_MUSEUM_IDS is not set
    # CONFIG_MTD_NAND_GPIO is not set
    CONFIG_MTD_NAND_IDS=y
    # CONFIG_MTD_NAND_DISKONCHIP is not set
    # CONFIG_MTD_NAND_NANDSIM is not set
    # CONFIG_MTD_NAND_PLATFORM is not set
    CONFIG_MTD_NAND_DAVINCI=y
    # CONFIG_MTD_ONENAND is not set

    #
    # LPDDR flash memory drivers
    #
    # CONFIG_MTD_LPDDR is not set
    # CONFIG_MTD_UBI is not set
    # CONFIG_PARPORT is not set
    CONFIG_BLK_DEV=y
    # CONFIG_BLK_DEV_COW_COMMON is not set
    CONFIG_BLK_DEV_LOOP=m
    # CONFIG_BLK_DEV_CRYPTOLOOP is not set

    #
    # DRBD disabled because PROC_FS, INET or CONNECTOR not selected
    #
    # CONFIG_BLK_DEV_NBD is not set
    CONFIG_BLK_DEV_RAM=y
    CONFIG_BLK_DEV_RAM_COUNT=1
    CONFIG_BLK_DEV_RAM_SIZE=32768
    # CONFIG_BLK_DEV_XIP is not set
    # CONFIG_CDROM_PKTCDVD is not set
    # CONFIG_ATA_OVER_ETH is not set
    # CONFIG_MG_DISK is not set
    # CONFIG_BLK_DEV_RBD is not set
    CONFIG_MISC_DEVICES=y
    # CONFIG_AD525X_DPOT is not set
    # CONFIG_ICS932S401 is not set
    # CONFIG_ENCLOSURE_SERVICES is not set
    # CONFIG_APDS9802ALS is not set
    # CONFIG_ISL29003 is not set
    # CONFIG_ISL29020 is not set
    # CONFIG_SENSORS_TSL2550 is not set
    # CONFIG_SENSORS_BH1780 is not set
    # CONFIG_SENSORS_BH1770 is not set
    # CONFIG_SENSORS_APDS990X is not set
    # CONFIG_HMC6352 is not set
    # CONFIG_DS1682 is not set
    # CONFIG_TI_DAC7512 is not set
    # CONFIG_BMP085 is not set
    # CONFIG_C2PORT is not set

    #
    # EEPROM support
    #
    CONFIG_EEPROM_AT24=y
    CONFIG_EEPROM_AT25=y
    # CONFIG_EEPROM_LEGACY is not set
    # CONFIG_EEPROM_MAX6875 is not set
    # CONFIG_EEPROM_93CX6 is not set
    # CONFIG_IWMC3200TOP is not set

    #
    # Texas Instruments shared transport line discipline
    #
    CONFIG_HAVE_IDE=y
    # CONFIG_IDE is not set

    #
    # SCSI device support
    #
    CONFIG_SCSI_MOD=y
    # CONFIG_RAID_ATTRS is not set
    CONFIG_SCSI=y
    CONFIG_SCSI_DMA=y
    # CONFIG_SCSI_TGT is not set
    # CONFIG_SCSI_NETLINK is not set
    CONFIG_SCSI_PROC_FS=y

    #
    # SCSI support type (disk, tape, CD-ROM)
    #
    CONFIG_BLK_DEV_SD=y
    # CONFIG_CHR_DEV_ST is not set
    # CONFIG_CHR_DEV_OSST is not set
    # CONFIG_BLK_DEV_SR is not set
    # CONFIG_CHR_DEV_SG is not set
    # CONFIG_CHR_DEV_SCH is not set
    # CONFIG_SCSI_MULTI_LUN is not set
    # CONFIG_SCSI_CONSTANTS is not set
    # CONFIG_SCSI_LOGGING is not set
    # CONFIG_SCSI_SCAN_ASYNC is not set
    CONFIG_SCSI_WAIT_SCAN=m

    #
    # SCSI Transports
    #
    # CONFIG_SCSI_SPI_ATTRS is not set
    # CONFIG_SCSI_FC_ATTRS is not set
    # CONFIG_SCSI_ISCSI_ATTRS is not set
    # CONFIG_SCSI_SAS_ATTRS is not set
    # CONFIG_SCSI_SAS_LIBSAS is not set
    # CONFIG_SCSI_SRP_ATTRS is not set
    CONFIG_SCSI_LOWLEVEL=y
    # CONFIG_ISCSI_TCP is not set
    # CONFIG_ISCSI_BOOT_SYSFS is not set
    # CONFIG_LIBFC is not set
    # CONFIG_LIBFCOE is not set
    # CONFIG_SCSI_DEBUG is not set
    # CONFIG_SCSI_DH is not set
    # CONFIG_SCSI_OSD_INITIATOR is not set
    # CONFIG_ATA is not set
    # CONFIG_MD is not set
    CONFIG_NETDEVICES=y
    # CONFIG_DUMMY is not set
    # CONFIG_BONDING is not set
    # CONFIG_MACVLAN is not set
    # CONFIG_EQUALIZER is not set
    CONFIG_TUN=m
    # CONFIG_VETH is not set
    # CONFIG_MII is not set
    CONFIG_PHYLIB=y

    #
    # MII PHY device drivers
    #
    # CONFIG_MARVELL_PHY is not set
    # CONFIG_DAVICOM_PHY is not set
    # CONFIG_QSEMI_PHY is not set
    CONFIG_LXT_PHY=y
    # CONFIG_CICADA_PHY is not set
    # CONFIG_VITESSE_PHY is not set
    # CONFIG_SMSC_PHY is not set
    # CONFIG_BROADCOM_PHY is not set
    # CONFIG_BCM63XX_PHY is not set
    # CONFIG_ICPLUS_PHY is not set
    # CONFIG_REALTEK_PHY is not set
    # CONFIG_NATIONAL_PHY is not set
    # CONFIG_STE10XP is not set
    CONFIG_LSI_ET1011C_PHY=y
    # CONFIG_MICREL_PHY is not set
    # CONFIG_FIXED_PHY is not set
    # CONFIG_MDIO_BITBANG is not set
    CONFIG_NET_ETHERNET=y
    # CONFIG_AX88796 is not set
    # CONFIG_SMC91X is not set
    CONFIG_TI_DAVINCI_EMAC=y
    CONFIG_TI_DAVINCI_MDIO=y
    CONFIG_TI_DAVINCI_CPDMA=y
    # CONFIG_DM9000 is not set
    # CONFIG_ENC28J60 is not set
    # CONFIG_ETHOC is not set
    # CONFIG_SMC911X is not set
    # CONFIG_SMSC911X is not set
    # CONFIG_DNET is not set
    # CONFIG_IBM_NEW_EMAC_ZMII is not set
    # CONFIG_IBM_NEW_EMAC_RGMII is not set
    # CONFIG_IBM_NEW_EMAC_TAH is not set
    # CONFIG_IBM_NEW_EMAC_EMAC4 is not set
    # CONFIG_IBM_NEW_EMAC_NO_FLOW_CTRL is not set
    # CONFIG_IBM_NEW_EMAC_MAL_CLR_ICINTSTAT is not set
    # CONFIG_IBM_NEW_EMAC_MAL_COMMON_ERR is not set
    # CONFIG_B44 is not set
    # CONFIG_KS8851 is not set
    # CONFIG_KS8851_MLL is not set
    # CONFIG_NETDEV_1000 is not set
    # CONFIG_NETDEV_10000 is not set
    CONFIG_WLAN=y
    # CONFIG_ATH_COMMON is not set
    # CONFIG_HOSTAP is not set
    # CONFIG_IWM is not set
    CONFIG_LIBERTAS=m
    CONFIG_LIBERTAS_SDIO=m
    # CONFIG_LIBERTAS_SPI is not set
    CONFIG_LIBERTAS_DEBUG=y
    # CONFIG_LIBERTAS_MESH is not set

    #
    # Enable WiMAX (Networking options) to see the WiMAX drivers
    #
    # CONFIG_WAN is not set

    #
    # CAIF transport drivers
    #
    CONFIG_PPP=m
    # CONFIG_PPP_MULTILINK is not set
    # CONFIG_PPP_FILTER is not set
    CONFIG_PPP_ASYNC=m
    CONFIG_PPP_SYNC_TTY=m
    CONFIG_PPP_DEFLATE=m
    # CONFIG_PPP_BSDCOMP is not set
    # CONFIG_PPP_MPPE is not set
    # CONFIG_PPPOE is not set
    # CONFIG_SLIP is not set
    CONFIG_SLHC=m
    CONFIG_NETCONSOLE=y
    # CONFIG_NETCONSOLE_DYNAMIC is not set
    CONFIG_NETPOLL=y
    CONFIG_NETPOLL_TRAP=y
    CONFIG_NET_POLL_CONTROLLER=y
    # CONFIG_ISDN is not set
    # CONFIG_PHONE is not set

    #
    # Input device support
    #
    CONFIG_INPUT=y
    CONFIG_INPUT_FF_MEMLESS=y
    # CONFIG_INPUT_POLLDEV is not set
    # CONFIG_INPUT_SPARSEKMAP is not set

    #
    # Userland interfaces
    #
    CONFIG_INPUT_MOUSEDEV=y
    # CONFIG_INPUT_MOUSEDEV_PSAUX is not set
    CONFIG_INPUT_MOUSEDEV_SCREEN_X=1024
    CONFIG_INPUT_MOUSEDEV_SCREEN_Y=768
    # CONFIG_INPUT_JOYDEV is not set
    CONFIG_INPUT_EVDEV=y
    CONFIG_INPUT_EVBUG=y

    #
    # Input Device Drivers
    #
    # CONFIG_INPUT_KEYBOARD is not set
    # CONFIG_INPUT_MOUSE is not set
    # CONFIG_INPUT_JOYSTICK is not set
    # CONFIG_INPUT_TABLET is not set
    CONFIG_INPUT_TOUCHSCREEN=y
    # CONFIG_TOUCHSCREEN_ADS7846 is not set
    # CONFIG_TOUCHSCREEN_AD7877 is not set
    # CONFIG_TOUCHSCREEN_AD7879 is not set
    # CONFIG_TOUCHSCREEN_BU21013 is not set
    # CONFIG_TOUCHSCREEN_CY8CTMG110 is not set
    # CONFIG_TOUCHSCREEN_DYNAPRO is not set
    # CONFIG_TOUCHSCREEN_HAMPSHIRE is not set
    # CONFIG_TOUCHSCREEN_EETI is not set
    # CONFIG_TOUCHSCREEN_FUJITSU is not set
    # CONFIG_TOUCHSCREEN_GUNZE is not set
    # CONFIG_TOUCHSCREEN_ELO is not set
    # CONFIG_TOUCHSCREEN_WACOM_W8001 is not set
    # CONFIG_TOUCHSCREEN_MCS5000 is not set
    # CONFIG_TOUCHSCREEN_MTOUCH is not set
    # CONFIG_TOUCHSCREEN_INEXIO is not set
    # CONFIG_TOUCHSCREEN_MK712 is not set
    # CONFIG_TOUCHSCREEN_PENMOUNT is not set
    # CONFIG_TOUCHSCREEN_QT602240 is not set
    # CONFIG_TOUCHSCREEN_TOUCHRIGHT is not set
    # CONFIG_TOUCHSCREEN_TOUCHWIN is not set
    # CONFIG_TOUCHSCREEN_USB_COMPOSITE is not set
    # CONFIG_TOUCHSCREEN_TOUCHIT213 is not set
    # CONFIG_TOUCHSCREEN_TSC2007 is not set
    CONFIG_TOUCHSCREEN_TSC2004=y
    # CONFIG_TOUCHSCREEN_W90X900 is not set
    # CONFIG_TOUCHSCREEN_TPS6507X is not set
    CONFIG_INPUT_MISC=y
    # CONFIG_INPUT_AD714X is not set
    # CONFIG_INPUT_ATI_REMOTE is not set
    # CONFIG_INPUT_ATI_REMOTE2 is not set
    # CONFIG_INPUT_KEYSPAN_REMOTE is not set
    # CONFIG_INPUT_POWERMATE is not set
    # CONFIG_INPUT_YEALINK is not set
    # CONFIG_INPUT_CM109 is not set
    # CONFIG_INPUT_UINPUT is not set
    # CONFIG_INPUT_PCF8574 is not set
    # CONFIG_INPUT_GPIO_ROTARY_ENCODER is not set
    CONFIG_INPUT_DM365EVM=y
    # CONFIG_INPUT_ADXL34X is not set

    #
    # Hardware I/O ports
    #
    CONFIG_SERIO=y
    CONFIG_SERIO_SERPORT=y
    CONFIG_SERIO_LIBPS2=y
    # CONFIG_SERIO_RAW is not set
    # CONFIG_SERIO_ALTERA_PS2 is not set
    # CONFIG_SERIO_PS2MULT is not set
    # CONFIG_GAMEPORT is not set

    #
    # Character devices
    #
    CONFIG_VT=y
    CONFIG_CONSOLE_TRANSLATIONS=y
    # CONFIG_VT_CONSOLE is not set
    CONFIG_HW_CONSOLE=y
    # CONFIG_VT_HW_CONSOLE_BINDING is not set
    CONFIG_DEVKMEM=y
    # CONFIG_SERIAL_NONSTANDARD is not set
    # CONFIG_N_GSM is not set

    #
    # Serial drivers
    #
    CONFIG_SERIAL_8250=y
    CONFIG_SERIAL_8250_CONSOLE=y
    CONFIG_SERIAL_8250_NR_UARTS=2
    CONFIG_SERIAL_8250_RUNTIME_UARTS=2
    # CONFIG_SERIAL_8250_EXTENDED is not set

    #
    # Non-8250 serial port support
    #
    # CONFIG_SERIAL_MAX3100 is not set
    # CONFIG_SERIAL_MAX3107 is not set
    CONFIG_SERIAL_CORE=y
    CONFIG_SERIAL_CORE_CONSOLE=y
    # CONFIG_SERIAL_TIMBERDALE is not set
    # CONFIG_SERIAL_ALTERA_JTAGUART is not set
    # CONFIG_SERIAL_ALTERA_UART is not set
    CONFIG_UNIX98_PTYS=y
    # CONFIG_DEVPTS_MULTIPLE_INSTANCES is not set
    CONFIG_LEGACY_PTYS=y
    CONFIG_LEGACY_PTY_COUNT=256
    # CONFIG_TTY_PRINTK is not set
    # CONFIG_IPMI_HANDLER is not set
    # CONFIG_HW_RANDOM is not set
    # CONFIG_R3964 is not set
    # CONFIG_RAW_DRIVER is not set
    # CONFIG_TCG_TPM is not set
    # CONFIG_RAMOOPS is not set
    CONFIG_I2C=y
    CONFIG_I2C_BOARDINFO=y
    CONFIG_I2C_COMPAT=y
    CONFIG_I2C_CHARDEV=y
    # CONFIG_I2C_MUX is not set
    CONFIG_I2C_HELPER_AUTO=y

    #
    # I2C Hardware Bus support
    #

    #
    # I2C system bus drivers (mostly embedded / system-on-chip)
    #
    CONFIG_I2C_DAVINCI=y
    # CONFIG_I2C_DESIGNWARE is not set
    # CONFIG_I2C_GPIO is not set
    # CONFIG_I2C_OCORES is not set
    # CONFIG_I2C_PCA_PLATFORM is not set
    # CONFIG_I2C_SIMTEC is not set
    # CONFIG_I2C_XILINX is not set

    #
    # External I2C/SMBus adapter drivers
    #
    # CONFIG_I2C_PARPORT_LIGHT is not set
    # CONFIG_I2C_TAOS_EVM is not set

    #
    # Other I2C/SMBus bus drivers
    #
    # CONFIG_I2C_STUB is not set
    # CONFIG_I2C_DEBUG_CORE is not set
    # CONFIG_I2C_DEBUG_ALGO is not set
    # CONFIG_I2C_DEBUG_BUS is not set
    CONFIG_SPI=y
    # CONFIG_SPI_DEBUG is not set
    CONFIG_SPI_MASTER=y

    #
    # SPI Master Controller Drivers
    #
    CONFIG_SPI_BITBANG=y
    CONFIG_SPI_DAVINCI=y
    # CONFIG_SPI_GPIO is not set
    # CONFIG_SPI_XILINX is not set
    # CONFIG_SPI_DESIGNWARE is not set

    #
    # SPI Protocol Masters
    #
    # CONFIG_SPI_SPIDEV is not set
    # CONFIG_SPI_TLE62X0 is not set

    #
    # PPS support
    #
    # CONFIG_PPS is not set
    CONFIG_ARCH_REQUIRE_GPIOLIB=y
    CONFIG_GPIOLIB=y
    # CONFIG_DEBUG_GPIO is not set
    # CONFIG_GPIO_SYSFS is not set

    #
    # Memory mapped GPIO expanders:
    #
    # CONFIG_GPIO_BASIC_MMIO is not set
    # CONFIG_GPIO_IT8761E is not set
    # CONFIG_GPIO_VX855 is not set

    #
    # I2C GPIO expanders:
    #
    # CONFIG_GPIO_MAX7300 is not set
    # CONFIG_GPIO_MAX732X is not set
    CONFIG_GPIO_PCF857X=y
    # CONFIG_GPIO_SX150X is not set
    # CONFIG_GPIO_ADP5588 is not set

    #
    # PCI GPIO expanders:
    #

    #
    # SPI GPIO expanders:
    #
    # CONFIG_GPIO_MAX7301 is not set
    # CONFIG_GPIO_MCP23S08 is not set
    # CONFIG_GPIO_MC33880 is not set
    # CONFIG_GPIO_74X164 is not set

    #
    # AC97 GPIO expanders:
    #

    #
    # MODULbus GPIO expanders:
    #
    # CONFIG_GENERIC_PWM is not set
    # CONFIG_W1 is not set
    # CONFIG_POWER_SUPPLY is not set
    CONFIG_HWMON=y
    # CONFIG_HWMON_VID is not set
    # CONFIG_HWMON_DEBUG_CHIP is not set

    #
    # Native drivers
    #
    # CONFIG_SENSORS_AD7414 is not set
    # CONFIG_SENSORS_AD7418 is not set
    # CONFIG_SENSORS_ADCXX is not set
    # CONFIG_SENSORS_ADM1021 is not set
    # CONFIG_SENSORS_ADM1025 is not set
    # CONFIG_SENSORS_ADM1026 is not set
    # CONFIG_SENSORS_ADM1029 is not set
    # CONFIG_SENSORS_ADM1031 is not set
    # CONFIG_SENSORS_ADM9240 is not set
    # CONFIG_SENSORS_ADT7411 is not set
    # CONFIG_SENSORS_ADT7462 is not set
    # CONFIG_SENSORS_ADT7470 is not set
    # CONFIG_SENSORS_ADT7475 is not set
    # CONFIG_SENSORS_ASC7621 is not set
    # CONFIG_SENSORS_ATXP1 is not set
    # CONFIG_SENSORS_DS1621 is not set
    # CONFIG_SENSORS_F71805F is not set
    # CONFIG_SENSORS_F71882FG is not set
    # CONFIG_SENSORS_F75375S is not set
    # CONFIG_SENSORS_G760A is not set
    # CONFIG_SENSORS_GL518SM is not set
    # CONFIG_SENSORS_GL520SM is not set
    # CONFIG_SENSORS_GPIO_FAN is not set
    # CONFIG_SENSORS_IT87 is not set
    # CONFIG_SENSORS_JC42 is not set
    # CONFIG_SENSORS_LM63 is not set
    # CONFIG_SENSORS_LM70 is not set
    # CONFIG_SENSORS_LM73 is not set
    # CONFIG_SENSORS_LM75 is not set
    # CONFIG_SENSORS_LM77 is not set
    # CONFIG_SENSORS_LM78 is not set
    # CONFIG_SENSORS_LM80 is not set
    # CONFIG_SENSORS_LM83 is not set
    # CONFIG_SENSORS_LM85 is not set
    # CONFIG_SENSORS_LM87 is not set
    # CONFIG_SENSORS_LM90 is not set
    # CONFIG_SENSORS_LM92 is not set
    # CONFIG_SENSORS_LM93 is not set
    # CONFIG_SENSORS_LTC4215 is not set
    # CONFIG_SENSORS_LTC4245 is not set
    # CONFIG_SENSORS_LTC4261 is not set
    # CONFIG_SENSORS_LM95241 is not set
    # CONFIG_SENSORS_MAX1111 is not set
    # CONFIG_SENSORS_MAX1619 is not set
    # CONFIG_SENSORS_MAX6650 is not set
    # CONFIG_SENSORS_PC87360 is not set
    # CONFIG_SENSORS_PC87427 is not set
    # CONFIG_SENSORS_PCF8591 is not set
    # CONFIG_SENSORS_SHT15 is not set
    # CONFIG_SENSORS_SMM665 is not set
    # CONFIG_SENSORS_DME1737 is not set
    # CONFIG_SENSORS_EMC1403 is not set
    # CONFIG_SENSORS_EMC2103 is not set
    # CONFIG_SENSORS_SMSC47M1 is not set
    # CONFIG_SENSORS_SMSC47M192 is not set
    # CONFIG_SENSORS_SMSC47B397 is not set
    # CONFIG_SENSORS_ADS7828 is not set
    # CONFIG_SENSORS_ADS7871 is not set
    # CONFIG_SENSORS_AMC6821 is not set
    # CONFIG_SENSORS_THMC50 is not set
    # CONFIG_SENSORS_TMP102 is not set
    # CONFIG_SENSORS_TMP401 is not set
    # CONFIG_SENSORS_TMP421 is not set
    # CONFIG_SENSORS_VT1211 is not set
    # CONFIG_SENSORS_W83781D is not set
    # CONFIG_SENSORS_W83791D is not set
    # CONFIG_SENSORS_W83792D is not set
    # CONFIG_SENSORS_W83793 is not set
    # CONFIG_SENSORS_W83795 is not set
    # CONFIG_SENSORS_W83L785TS is not set
    # CONFIG_SENSORS_W83L786NG is not set
    # CONFIG_SENSORS_W83627HF is not set
    # CONFIG_SENSORS_W83627EHF is not set
    # CONFIG_SENSORS_LIS3_SPI is not set
    # CONFIG_SENSORS_LIS3_I2C is not set
    # CONFIG_THERMAL is not set
    CONFIG_WATCHDOG=y
    # CONFIG_WATCHDOG_NOWAYOUT is not set

    #
    # Watchdog Device Drivers
    #
    # CONFIG_SOFT_WATCHDOG is not set
    CONFIG_DAVINCI_WATCHDOG=y
    # CONFIG_MAX63XX_WATCHDOG is not set
    CONFIG_SSB_POSSIBLE=y

    #
    # Sonics Silicon Backplane
    #
    # CONFIG_SSB is not set
    CONFIG_MFD_SUPPORT=y
    # CONFIG_MFD_CORE is not set
    # CONFIG_MFD_88PM860X is not set
    # CONFIG_MFD_SM501 is not set
    # CONFIG_MFD_ASIC3 is not set
    # CONFIG_HTC_EGPIO is not set
    # CONFIG_HTC_PASIC3 is not set
    # CONFIG_HTC_I2CPLD is not set
    # CONFIG_TPS65010 is not set
    # CONFIG_TPS6507X is not set
    # CONFIG_TWL4030_CORE is not set
    # CONFIG_MFD_STMPE is not set
    # CONFIG_MFD_TC35892 is not set
    # CONFIG_MFD_TMIO is not set
    # CONFIG_MFD_T7L66XB is not set
    # CONFIG_MFD_TC6387XB is not set
    # CONFIG_MFD_TC6393XB is not set
    # CONFIG_PMIC_DA903X is not set
    # CONFIG_PMIC_ADP5520 is not set
    # CONFIG_MFD_MAX8925 is not set
    # CONFIG_MFD_MAX8998 is not set
    # CONFIG_MFD_WM8400 is not set
    # CONFIG_MFD_WM831X_I2C is not set
    # CONFIG_MFD_WM831X_SPI is not set
    # CONFIG_MFD_WM8350_I2C is not set
    # CONFIG_MFD_WM8994 is not set
    # CONFIG_MFD_PCF50633 is not set
    # CONFIG_MFD_MC13XXX is not set
    # CONFIG_ABX500_CORE is not set
    # CONFIG_EZX_PCAP is not set
    # CONFIG_MFD_TPS6586X is not set
    # CONFIG_REGULATOR is not set
    CONFIG_MEDIA_SUPPORT=y

    #
    # Multimedia core support
    #
    CONFIG_MEDIA_CONTROLLER=y
    CONFIG_VIDEO_DEV=y
    CONFIG_VIDEO_V4L2_COMMON=y
    # CONFIG_VIDEO_ALLOW_V4L1 is not set
    # CONFIG_VIDEO_V4L1_COMPAT is not set
    CONFIG_VIDEO_V4L2_SUBDEV_API=y
    # CONFIG_DVB_CORE is not set
    CONFIG_VIDEO_MEDIA=y

    #
    # Multimedia drivers
    #
    CONFIG_IR_CORE=y
    CONFIG_VIDEO_IR=y
    CONFIG_LIRC=y
    CONFIG_RC_MAP=y
    CONFIG_IR_NEC_DECODER=y
    CONFIG_IR_RC5_DECODER=y
    CONFIG_IR_RC6_DECODER=y
    CONFIG_IR_JVC_DECODER=y
    CONFIG_IR_SONY_DECODER=y
    CONFIG_IR_RC5_SZ_DECODER=y
    CONFIG_IR_LIRC_CODEC=y
    # CONFIG_IR_IMON is not set
    # CONFIG_IR_MCEUSB is not set
    # CONFIG_IR_STREAMZAP is not set
    # CONFIG_MEDIA_ATTACH is not set
    CONFIG_MEDIA_TUNER=y
    # CONFIG_MEDIA_TUNER_CUSTOMISE is not set
    CONFIG_MEDIA_TUNER_SIMPLE=y
    CONFIG_MEDIA_TUNER_TDA8290=y
    CONFIG_MEDIA_TUNER_TDA827X=y
    CONFIG_MEDIA_TUNER_TDA18271=y
    CONFIG_MEDIA_TUNER_TDA9887=y
    CONFIG_MEDIA_TUNER_TEA5761=y
    CONFIG_MEDIA_TUNER_TEA5767=y
    CONFIG_MEDIA_TUNER_MT20XX=y
    CONFIG_MEDIA_TUNER_XC2028=y
    CONFIG_MEDIA_TUNER_XC5000=y
    CONFIG_MEDIA_TUNER_MC44S803=y
    CONFIG_VIDEO_V4L2=y
    CONFIG_VIDEOBUF_GEN=y
    CONFIG_VIDEOBUF_DMA_CONTIG=y
    CONFIG_VIDEO_CAPTURE_DRIVERS=y
    # CONFIG_VIDEO_ADV_DEBUG is not set
    # CONFIG_VIDEO_FIXED_MINOR_RANGES is not set
    # CONFIG_VIDEO_HELPER_CHIPS_AUTO is not set
    CONFIG_VIDEO_IR_I2C=y

    #
    # Encoders/decoders and other helper chips
    #

    #
    # Audio decoders
    #
    # CONFIG_VIDEO_TVAUDIO is not set
    # CONFIG_VIDEO_TDA7432 is not set
    # CONFIG_VIDEO_TDA9840 is not set
    # CONFIG_VIDEO_TDA9875 is not set
    # CONFIG_VIDEO_TEA6415C is not set
    # CONFIG_VIDEO_TEA6420 is not set
    # CONFIG_VIDEO_MSP3400 is not set
    # CONFIG_VIDEO_CS5345 is not set
    # CONFIG_VIDEO_CS53L32A is not set
    # CONFIG_VIDEO_M52790 is not set
    # CONFIG_VIDEO_TLV320AIC23B is not set
    # CONFIG_VIDEO_WM8775 is not set
    # CONFIG_VIDEO_WM8739 is not set
    # CONFIG_VIDEO_VP27SMPX is not set

    #
    # RDS decoders
    #
    # CONFIG_VIDEO_SAA6588 is not set

    #
    # Video decoders
    #
    # CONFIG_VIDEO_ADV7180 is not set
    # CONFIG_VIDEO_BT819 is not set
    # CONFIG_VIDEO_BT856 is not set
    # CONFIG_VIDEO_BT866 is not set
    # CONFIG_VIDEO_KS0127 is not set
    # CONFIG_VIDEO_OV7670 is not set
    # CONFIG_VIDEO_MT9V011 is not set
    # CONFIG_VIDEO_TCM825X is not set
    # CONFIG_VIDEO_SAA7110 is not set
    # CONFIG_VIDEO_SAA711X is not set
    # CONFIG_VIDEO_SAA717X is not set
    # CONFIG_VIDEO_SAA7191 is not set
    CONFIG_VIDEO_TVP514X=y
    # CONFIG_VIDEO_TVP5150 is not set
    CONFIG_VIDEO_TVP7002=y
    # CONFIG_VIDEO_VPX3220 is not set

    #
    # Video and audio decoders
    #
    # CONFIG_VIDEO_CX25840 is not set

    #
    # MPEG video encoders
    #
    # CONFIG_VIDEO_CX2341X is not set

    #
    # Video encoders
    #
    # CONFIG_VIDEO_SAA7127 is not set
    # CONFIG_VIDEO_SAA7185 is not set
    # CONFIG_VIDEO_ADV7170 is not set
    # CONFIG_VIDEO_ADV7175 is not set
    CONFIG_VIDEO_THS7303=y
    CONFIG_VIDEO_THS7353=y
    # CONFIG_VIDEO_ADV7343 is not set
    # CONFIG_VIDEO_AK881X is not set

    #
    # Video improvement chips
    #
    # CONFIG_VIDEO_UPD64031A is not set
    # CONFIG_VIDEO_UPD64083 is not set
    # CONFIG_VIDEO_VIVI is not set
    CONFIG_VIDEO_DM365_3A_HW=y
    CONFIG_VIDEO_DM365_AF=y
    CONFIG_VIDEO_DM365_AEW=y
    CONFIG_DM365_IPIPE=y
    # CONFIG_IMP_DEBUG is not set
    CONFIG_VIDEO_VPSS_SYSTEM=y
    CONFIG_VIDEO_VPFE_CAPTURE=y
    CONFIG_VIDEO_ISIF=y
    CONFIG_VIDEO_DM644X_VPBE=y
    CONFIG_VIDEO_VPBE_DISPLAY=y
    CONFIG_VIDEO_VPBE_FB=y
    # CONFIG_VIDEO_SR030PC30 is not set
    # CONFIG_SOC_CAMERA is not set
    # CONFIG_SOC_CAMERA_MT9T031 is not set
    CONFIG_SOC_CAMERA_MT9P031=y
    # CONFIG_V4L_MEM2MEM_DRIVERS is not set
    # CONFIG_RADIO_ADAPTERS is not set
    # CONFIG_DAB is not set

    #
    # Graphics support
    #
    # CONFIG_DRM is not set
    # CONFIG_VGASTATE is not set
    CONFIG_VIDEO_OUTPUT_CONTROL=y
    CONFIG_FB=y
    # CONFIG_FIRMWARE_EDID is not set
    # CONFIG_FB_DDC is not set
    # CONFIG_FB_BOOT_VESA_SUPPORT is not set
    CONFIG_FB_CFB_FILLRECT=y
    CONFIG_FB_CFB_COPYAREA=y
    CONFIG_FB_CFB_IMAGEBLIT=y
    # CONFIG_FB_CFB_REV_PIXELS_IN_BYTE is not set
    # CONFIG_FB_SYS_FILLRECT is not set
    # CONFIG_FB_SYS_COPYAREA is not set
    # CONFIG_FB_SYS_IMAGEBLIT is not set
    # CONFIG_FB_FOREIGN_ENDIAN is not set
    # CONFIG_FB_SYS_FOPS is not set
    # CONFIG_FB_SVGALIB is not set
    # CONFIG_FB_MACMODES is not set
    # CONFIG_FB_BACKLIGHT is not set
    # CONFIG_FB_MODE_HELPERS is not set
    # CONFIG_FB_TILEBLITTING is not set

    #
    # Frame buffer hardware drivers
    #
    # CONFIG_FB_S1D13XXX is not set
    # CONFIG_FB_VIRTUAL is not set
    # CONFIG_FB_METRONOME is not set
    # CONFIG_FB_MB862XX is not set
    # CONFIG_FB_BROADSHEET is not set
    # CONFIG_BACKLIGHT_LCD_SUPPORT is not set

    #
    # Display device support
    #
    # CONFIG_DISPLAY_SUPPORT is not set

    #
    # Console display driver support
    #
    CONFIG_DUMMY_CONSOLE=y
    CONFIG_FRAMEBUFFER_CONSOLE=y
    # CONFIG_FRAMEBUFFER_CONSOLE_DETECT_PRIMARY is not set
    # CONFIG_FRAMEBUFFER_CONSOLE_ROTATION is not set
    # CONFIG_FONTS is not set
    CONFIG_FONT_8x8=y
    CONFIG_FONT_8x16=y
    CONFIG_LOGO=y
    CONFIG_LOGO_LINUX_MONO=y
    CONFIG_LOGO_LINUX_VGA16=y
    CONFIG_LOGO_LINUX_CLUT224=y
    CONFIG_SOUND=y
    # CONFIG_SOUND_OSS_CORE is not set
    CONFIG_SND=y
    CONFIG_SND_TIMER=y
    CONFIG_SND_PCM=y
    CONFIG_SND_JACK=y
    # CONFIG_SND_SEQUENCER is not set
    # CONFIG_SND_MIXER_OSS is not set
    # CONFIG_SND_PCM_OSS is not set
    # CONFIG_SND_HRTIMER is not set
    # CONFIG_SND_DYNAMIC_MINORS is not set
    CONFIG_SND_SUPPORT_OLD_API=y
    CONFIG_SND_VERBOSE_PROCFS=y
    # CONFIG_SND_VERBOSE_PRINTK is not set
    # CONFIG_SND_DEBUG is not set
    # CONFIG_SND_RAWMIDI_SEQ is not set
    # CONFIG_SND_OPL3_LIB_SEQ is not set
    # CONFIG_SND_OPL4_LIB_SEQ is not set
    # CONFIG_SND_SBAWE_SEQ is not set
    # CONFIG_SND_EMU10K1_SEQ is not set
    CONFIG_SND_DRIVERS=y
    # CONFIG_SND_DUMMY is not set
    # CONFIG_SND_ALOOP is not set
    # CONFIG_SND_MTPAV is not set
    # CONFIG_SND_SERIAL_U16550 is not set
    # CONFIG_SND_MPU401 is not set
    CONFIG_SND_ARM=y
    CONFIG_SND_SPI=y
    CONFIG_SND_SOC=y
    CONFIG_SND_DAVINCI_SOC=y
    CONFIG_SND_DAVINCI_SOC_I2S=y
    CONFIG_SND_DAVINCI_SOC_EVM=y
    CONFIG_SND_DM365_AIC3X_CODEC=y
    # CONFIG_SND_DM365_VOICE_CODEC is not set
    CONFIG_SND_SOC_I2C_AND_SPI=y
    # CONFIG_SND_SOC_ALL_CODECS is not set
    CONFIG_SND_SOC_TLV320AIC3X=y
    # CONFIG_SOUND_PRIME is not set
    CONFIG_HID_SUPPORT=y
    CONFIG_HID=y
    # CONFIG_HIDRAW is not set
    # CONFIG_HID_PID is not set

    #
    # Special HID drivers
    #
    CONFIG_USB_SUPPORT=y
    CONFIG_USB_ARCH_HAS_HCD=y
    # CONFIG_USB_ARCH_HAS_OHCI is not set
    # CONFIG_USB_ARCH_HAS_EHCI is not set
    # CONFIG_USB is not set
    # CONFIG_USB_OTG_WHITELIST is not set
    # CONFIG_USB_OTG_BLACKLIST_HUB is not set
    CONFIG_USB_MUSB_HDRC=y

    #
    # Platform Glue Layer
    #
    CONFIG_USB_MUSB_DAVINCI_GLUE=y
    CONFIG_USB_MUSB_DAVINCI=y
    # CONFIG_USB_MUSB_DA8XX is not set
    # CONFIG_USB_MUSB_TUSB6010 is not set
    # CONFIG_USB_MUSB_OMAP2PLUS is not set
    # CONFIG_USB_MUSB_AM35X is not set
    # CONFIG_USB_MUSB_BLACKFIN is not set
    # CONFIG_USB_MUSB_UX500 is not set
    CONFIG_USB_MUSB_PERIPHERAL=y
    CONFIG_USB_GADGET_MUSB_HDRC=y
    # CONFIG_MUSB_PIO_ONLY is not set
    # CONFIG_USB_INVENTRA_DMA_HW is not set
    CONFIG_USB_TI_CPPI_DMA_HW=y
    # CONFIG_USB_TI_CPPI41_DMA_HW is not set
    # CONFIG_USB_INVENTRA_DMA is not set
    CONFIG_USB_TI_CPPI_DMA=y
    # CONFIG_USB_TI_CPPI41_DMA is not set
    # CONFIG_USB_TUSB_OMAP_DMA is not set
    CONFIG_USB_MUSB_DEBUG=y

    #
    # NOTE: USB_STORAGE depends on SCSI but BLK_DEV_SD may
    #
    CONFIG_USB_GADGET=y
    # CONFIG_USB_GADGET_DEBUG is not set
    # CONFIG_USB_GADGET_DEBUG_FILES is not set
    # CONFIG_USB_GADGET_DEBUG_FS is not set
    CONFIG_USB_GADGET_VBUS_DRAW=2
    CONFIG_USB_GADGET_SELECTED=y
    # CONFIG_USB_GADGET_R8A66597 is not set
    # CONFIG_USB_GADGET_M66592 is not set
    CONFIG_USB_GADGET_DUALSPEED=y
    # CONFIG_USB_ZERO is not set
    # CONFIG_USB_AUDIO is not set
    # CONFIG_USB_ETH is not set
    # CONFIG_USB_GADGETFS is not set
    # CONFIG_USB_FUNCTIONFS is not set
    # CONFIG_USB_FILE_STORAGE is not set
    # CONFIG_USB_MASS_STORAGE is not set
    # CONFIG_USB_G_SERIAL is not set
    # CONFIG_USB_MIDI_GADGET is not set
    # CONFIG_USB_G_PRINTER is not set
    # CONFIG_USB_CDC_COMPOSITE is not set
    # CONFIG_USB_G_MULTI is not set
    # CONFIG_USB_G_HID is not set
    # CONFIG_USB_G_DBGP is not set
    CONFIG_USB_G_WEBCAM=m

    #
    # OTG and related infrastructure
    #
    CONFIG_USB_OTG_UTILS=y
    # CONFIG_USB_GPIO_VBUS is not set
    # CONFIG_USB_ULPI is not set
    CONFIG_NOP_USB_XCEIV=y
    CONFIG_MMC=y
    # CONFIG_MMC_DEBUG is not set
    # CONFIG_MMC_UNSAFE_RESUME is not set

    #
    # MMC/SD/SDIO Card Drivers
    #
    CONFIG_MMC_BLOCK=y
    CONFIG_MMC_BLOCK_MINORS=8
    # CONFIG_MMC_BLOCK_BOUNCE is not set
    CONFIG_SDIO_UART=y
    # CONFIG_MMC_TEST is not set

    #
    # MMC/SD/SDIO Host Controller Drivers
    #
    # CONFIG_MMC_SDHCI is not set
    CONFIG_MMC_DAVINCI=y
    # CONFIG_MMC_SPI is not set
    # CONFIG_MEMSTICK is not set
    CONFIG_NEW_LEDS=y
    CONFIG_LEDS_CLASS=y

    #
    # LED drivers
    #
    # CONFIG_LEDS_PCA9532 is not set
    CONFIG_LEDS_GPIO=m
    CONFIG_LEDS_GPIO_PLATFORM=y
    # CONFIG_LEDS_LP3944 is not set
    # CONFIG_LEDS_LP5521 is not set
    # CONFIG_LEDS_LP5523 is not set
    # CONFIG_LEDS_PCA955X is not set
    # CONFIG_LEDS_DAC124S085 is not set
    # CONFIG_LEDS_BD2802 is not set
    # CONFIG_LEDS_LT3593 is not set
    CONFIG_LEDS_TRIGGERS=y

    #
    # LED Triggers
    #
    CONFIG_LEDS_TRIGGER_TIMER=m
    CONFIG_LEDS_TRIGGER_HEARTBEAT=m
    # CONFIG_LEDS_TRIGGER_BACKLIGHT is not set
    # CONFIG_LEDS_TRIGGER_GPIO is not set
    # CONFIG_LEDS_TRIGGER_DEFAULT_ON is not set

    #
    # iptables trigger is under Netfilter config (LED target)
    #
    # CONFIG_ACCESSIBILITY is not set
    CONFIG_RTC_LIB=y
    # CONFIG_RTC_CLASS is not set
    # CONFIG_DMADEVICES is not set
    # CONFIG_AUXDISPLAY is not set
    # CONFIG_UIO is not set
    # CONFIG_STAGING is not set

    #
    # File systems
    #
    CONFIG_EXT2_FS=y
    # CONFIG_EXT2_FS_XATTR is not set
    # CONFIG_EXT2_FS_XIP is not set
    CONFIG_EXT3_FS=y
    # CONFIG_EXT3_DEFAULTS_TO_ORDERED is not set
    CONFIG_EXT3_FS_XATTR=y
    # CONFIG_EXT3_FS_POSIX_ACL is not set
    # CONFIG_EXT3_FS_SECURITY is not set
    # CONFIG_EXT4_FS is not set
    CONFIG_JBD=y
    # CONFIG_JBD_DEBUG is not set
    CONFIG_FS_MBCACHE=y
    # CONFIG_REISERFS_FS is not set
    # CONFIG_JFS_FS is not set
    # CONFIG_FS_POSIX_ACL is not set
    CONFIG_XFS_FS=m
    # CONFIG_XFS_QUOTA is not set
    # CONFIG_XFS_POSIX_ACL is not set
    # CONFIG_XFS_RT is not set
    # CONFIG_XFS_DEBUG is not set
    # CONFIG_GFS2_FS is not set
    # CONFIG_OCFS2_FS is not set
    # CONFIG_BTRFS_FS is not set
    # CONFIG_NILFS2_FS is not set
    CONFIG_EXPORTFS=m
    CONFIG_FILE_LOCKING=y
    CONFIG_FSNOTIFY=y
    CONFIG_DNOTIFY=y
    CONFIG_INOTIFY_USER=y
    # CONFIG_FANOTIFY is not set
    # CONFIG_QUOTA is not set
    # CONFIG_QUOTACTL is not set
    CONFIG_AUTOFS4_FS=m
    # CONFIG_FUSE_FS is not set

    #
    # Caches
    #
    # CONFIG_FSCACHE is not set

    #
    # CD-ROM/DVD Filesystems
    #
    # CONFIG_ISO9660_FS is not set
    # CONFIG_UDF_FS is not set

    #
    # DOS/FAT/NT Filesystems
    #
    CONFIG_FAT_FS=y
    CONFIG_MSDOS_FS=y
    CONFIG_VFAT_FS=y
    CONFIG_FAT_DEFAULT_CODEPAGE=437
    CONFIG_FAT_DEFAULT_IOCHARSET="iso8859-1"
    # CONFIG_NTFS_FS is not set

    #
    # Pseudo filesystems
    #
    CONFIG_PROC_FS=y
    CONFIG_PROC_SYSCTL=y
    CONFIG_PROC_PAGE_MONITOR=y
    CONFIG_SYSFS=y
    CONFIG_TMPFS=y
    # CONFIG_TMPFS_POSIX_ACL is not set
    # CONFIG_HUGETLB_PAGE is not set
    # CONFIG_CONFIGFS_FS is not set
    CONFIG_MISC_FILESYSTEMS=y
    # CONFIG_ADFS_FS is not set
    # CONFIG_AFFS_FS is not set
    # CONFIG_HFS_FS is not set
    # CONFIG_HFSPLUS_FS is not set
    # CONFIG_BEFS_FS is not set
    # CONFIG_BFS_FS is not set
    # CONFIG_EFS_FS is not set
    CONFIG_JFFS2_FS=y
    CONFIG_JFFS2_FS_DEBUG=0
    CONFIG_JFFS2_FS_WRITEBUFFER=y
    # CONFIG_JFFS2_FS_WBUF_VERIFY is not set
    # CONFIG_JFFS2_SUMMARY is not set
    # CONFIG_JFFS2_FS_XATTR is not set
    # CONFIG_JFFS2_COMPRESSION_OPTIONS is not set
    CONFIG_JFFS2_ZLIB=y
    # CONFIG_JFFS2_LZO is not set
    CONFIG_JFFS2_RTIME=y
    # CONFIG_JFFS2_RUBIN is not set
    # CONFIG_LOGFS is not set
    CONFIG_CRAMFS=y
    # CONFIG_SQUASHFS is not set
    # CONFIG_VXFS_FS is not set
    CONFIG_MINIX_FS=m
    # CONFIG_OMFS_FS is not set
    # CONFIG_HPFS_FS is not set
    # CONFIG_QNX4FS_FS is not set
    # CONFIG_ROMFS_FS is not set
    # CONFIG_SYSV_FS is not set
    # CONFIG_UFS_FS is not set
    CONFIG_NETWORK_FILESYSTEMS=y
    CONFIG_NFS_FS=y
    CONFIG_NFS_V3=y
    # CONFIG_NFS_V3_ACL is not set
    # CONFIG_NFS_V4 is not set
    CONFIG_ROOT_NFS=y
    CONFIG_NFSD=m
    CONFIG_NFSD_DEPRECATED=y
    CONFIG_NFSD_V3=y
    # CONFIG_NFSD_V3_ACL is not set
    # CONFIG_NFSD_V4 is not set
    CONFIG_LOCKD=y
    CONFIG_LOCKD_V4=y
    CONFIG_NFS_COMMON=y
    CONFIG_SUNRPC=y
    # CONFIG_RPCSEC_GSS_KRB5 is not set
    # CONFIG_CEPH_FS is not set
    # CONFIG_CIFS is not set
    # CONFIG_NCP_FS is not set
    # CONFIG_CODA_FS is not set
    # CONFIG_AFS_FS is not set

    #
    # Partition Types
    #
    CONFIG_PARTITION_ADVANCED=y
    # CONFIG_ACORN_PARTITION is not set
    # CONFIG_OSF_PARTITION is not set
    # CONFIG_AMIGA_PARTITION is not set
    # CONFIG_ATARI_PARTITION is not set
    # CONFIG_MAC_PARTITION is not set
    CONFIG_MSDOS_PARTITION=y
    # CONFIG_BSD_DISKLABEL is not set
    # CONFIG_MINIX_SUBPARTITION is not set
    # CONFIG_SOLARIS_X86_PARTITION is not set
    # CONFIG_UNIXWARE_DISKLABEL is not set
    # CONFIG_LDM_PARTITION is not set
    # CONFIG_SGI_PARTITION is not set
    # CONFIG_ULTRIX_PARTITION is not set
    # CONFIG_SUN_PARTITION is not set
    # CONFIG_KARMA_PARTITION is not set
    # CONFIG_EFI_PARTITION is not set
    # CONFIG_SYSV68_PARTITION is not set
    CONFIG_NLS=y
    CONFIG_NLS_DEFAULT="iso8859-1"
    CONFIG_NLS_CODEPAGE_437=y
    # CONFIG_NLS_CODEPAGE_737 is not set
    # CONFIG_NLS_CODEPAGE_775 is not set
    # CONFIG_NLS_CODEPAGE_850 is not set
    # CONFIG_NLS_CODEPAGE_852 is not set
    # CONFIG_NLS_CODEPAGE_855 is not set
    # CONFIG_NLS_CODEPAGE_857 is not set
    # CONFIG_NLS_CODEPAGE_860 is not set
    # CONFIG_NLS_CODEPAGE_861 is not set
    # CONFIG_NLS_CODEPAGE_862 is not set
    # CONFIG_NLS_CODEPAGE_863 is not set
    # CONFIG_NLS_CODEPAGE_864 is not set
    # CONFIG_NLS_CODEPAGE_865 is not set
    # CONFIG_NLS_CODEPAGE_866 is not set
    # CONFIG_NLS_CODEPAGE_869 is not set
    # CONFIG_NLS_CODEPAGE_936 is not set
    # CONFIG_NLS_CODEPAGE_950 is not set
    # CONFIG_NLS_CODEPAGE_932 is not set
    # CONFIG_NLS_CODEPAGE_949 is not set
    # CONFIG_NLS_CODEPAGE_874 is not set
    # CONFIG_NLS_ISO8859_8 is not set
    # CONFIG_NLS_CODEPAGE_1250 is not set
    # CONFIG_NLS_CODEPAGE_1251 is not set
    CONFIG_NLS_ASCII=m
    CONFIG_NLS_ISO8859_1=y
    # CONFIG_NLS_ISO8859_2 is not set
    # CONFIG_NLS_ISO8859_3 is not set
    # CONFIG_NLS_ISO8859_4 is not set
    # CONFIG_NLS_ISO8859_5 is not set
    # CONFIG_NLS_ISO8859_6 is not set
    # CONFIG_NLS_ISO8859_7 is not set
    # CONFIG_NLS_ISO8859_9 is not set
    # CONFIG_NLS_ISO8859_13 is not set
    # CONFIG_NLS_ISO8859_14 is not set
    # CONFIG_NLS_ISO8859_15 is not set
    # CONFIG_NLS_KOI8_R is not set
    # CONFIG_NLS_KOI8_U is not set
    CONFIG_NLS_UTF8=m
    # CONFIG_DLM is not set

    #
    # Kernel hacking
    #
    # CONFIG_PRINTK_TIME is not set
    CONFIG_ENABLE_WARN_DEPRECATED=y
    CONFIG_ENABLE_MUST_CHECK=y
    CONFIG_FRAME_WARN=1024
    # CONFIG_MAGIC_SYSRQ is not set
    # CONFIG_STRIP_ASM_SYMS is not set
    # CONFIG_UNUSED_SYMBOLS is not set
    CONFIG_DEBUG_FS=y
    # CONFIG_HEADERS_CHECK is not set
    CONFIG_DEBUG_KERNEL=y
    # CONFIG_DEBUG_SHIRQ is not set
    # CONFIG_LOCKUP_DETECTOR is not set
    # CONFIG_HARDLOCKUP_DETECTOR is not set
    CONFIG_DETECT_HUNG_TASK=y
    # CONFIG_BOOTPARAM_HUNG_TASK_PANIC is not set
    CONFIG_BOOTPARAM_HUNG_TASK_PANIC_VALUE=0
    CONFIG_SCHED_DEBUG=y
    # CONFIG_SCHEDSTATS is not set
    CONFIG_TIMER_STATS=y
    # CONFIG_DEBUG_OBJECTS is not set
    # CONFIG_SLUB_DEBUG_ON is not set
    # CONFIG_SLUB_STATS is not set
    # CONFIG_DEBUG_KMEMLEAK is not set
    CONFIG_DEBUG_PREEMPT=y
    CONFIG_DEBUG_RT_MUTEXES=y
    CONFIG_DEBUG_PI_LIST=y
    # CONFIG_RT_MUTEX_TESTER is not set
    # CONFIG_DEBUG_SPINLOCK is not set
    CONFIG_DEBUG_MUTEXES=y
    CONFIG_BKL=y
    # CONFIG_DEBUG_LOCK_ALLOC is not set
    # CONFIG_PROVE_LOCKING is not set
    # CONFIG_SPARSE_RCU_POINTER is not set
    # CONFIG_LOCK_STAT is not set
    # CONFIG_DEBUG_SPINLOCK_SLEEP is not set
    # CONFIG_DEBUG_LOCKING_API_SELFTESTS is not set
    # CONFIG_DEBUG_KOBJECT is not set
    CONFIG_DEBUG_BUGVERBOSE=y
    # CONFIG_DEBUG_INFO is not set
    # CONFIG_DEBUG_VM is not set
    # CONFIG_DEBUG_WRITECOUNT is not set
    # CONFIG_DEBUG_MEMORY_INIT is not set
    # CONFIG_DEBUG_LIST is not set
    # CONFIG_TEST_LIST_SORT is not set
    # CONFIG_DEBUG_SG is not set
    # CONFIG_DEBUG_NOTIFIERS is not set
    # CONFIG_DEBUG_CREDENTIALS is not set
    CONFIG_FRAME_POINTER=y
    # CONFIG_BOOT_PRINTK_DELAY is not set
    # CONFIG_RCU_TORTURE_TEST is not set
    # CONFIG_RCU_CPU_STALL_DETECTOR is not set
    # CONFIG_BACKTRACE_SELF_TEST is not set
    # CONFIG_DEBUG_BLOCK_EXT_DEVT is not set
    # CONFIG_DEBUG_FORCE_WEAK_PER_CPU is not set
    # CONFIG_LKDTM is not set
    # CONFIG_FAULT_INJECTION is not set
    # CONFIG_LATENCYTOP is not set
    # CONFIG_SYSCTL_SYSCALL_CHECK is not set
    # CONFIG_PAGE_POISONING is not set
    CONFIG_HAVE_FUNCTION_TRACER=y
    CONFIG_HAVE_DYNAMIC_FTRACE=y
    CONFIG_HAVE_FTRACE_MCOUNT_RECORD=y
    CONFIG_TRACING_SUPPORT=y
    CONFIG_FTRACE=y
    # CONFIG_FUNCTION_TRACER is not set
    # CONFIG_IRQSOFF_TRACER is not set
    # CONFIG_PREEMPT_TRACER is not set
    # CONFIG_SCHED_TRACER is not set
    # CONFIG_ENABLE_DEFAULT_TRACERS is not set
    CONFIG_BRANCH_PROFILE_NONE=y
    # CONFIG_PROFILE_ANNOTATED_BRANCHES is not set
    # CONFIG_PROFILE_ALL_BRANCHES is not set
    # CONFIG_STACK_TRACER is not set
    # CONFIG_BLK_DEV_IO_TRACE is not set
    # CONFIG_DYNAMIC_DEBUG is not set
    # CONFIG_ATOMIC64_SELFTEST is not set
    # CONFIG_SAMPLES is not set
    CONFIG_HAVE_ARCH_KGDB=y
    # CONFIG_KGDB is not set
    # CONFIG_STRICT_DEVMEM is not set
    # CONFIG_ARM_UNWIND is not set
    CONFIG_DEBUG_USER=y
    CONFIG_DEBUG_ERRORS=y
    # CONFIG_DEBUG_STACK_USAGE is not set
    # CONFIG_DEBUG_LL is not set
    # CONFIG_OC_ETM is not set

    #
    # Security options
    #
    # CONFIG_KEYS is not set
    # CONFIG_SECURITY_DMESG_RESTRICT is not set
    # CONFIG_SECURITY is not set
    # CONFIG_SECURITYFS is not set
    CONFIG_DEFAULT_SECURITY_DAC=y
    CONFIG_DEFAULT_SECURITY=""
    CONFIG_CRYPTO=y

    #
    # Crypto core or helper
    #
    CONFIG_CRYPTO_ALGAPI=y
    CONFIG_CRYPTO_ALGAPI2=y
    CONFIG_CRYPTO_AEAD2=y
    CONFIG_CRYPTO_BLKCIPHER=y
    CONFIG_CRYPTO_BLKCIPHER2=y
    CONFIG_CRYPTO_HASH2=y
    CONFIG_CRYPTO_RNG2=y
    CONFIG_CRYPTO_PCOMP2=y
    CONFIG_CRYPTO_MANAGER=y
    CONFIG_CRYPTO_MANAGER2=y
    CONFIG_CRYPTO_MANAGER_DISABLE_TESTS=y
    # CONFIG_CRYPTO_GF128MUL is not set
    # CONFIG_CRYPTO_NULL is not set
    CONFIG_CRYPTO_WORKQUEUE=y
    # CONFIG_CRYPTO_CRYPTD is not set
    # CONFIG_CRYPTO_AUTHENC is not set
    # CONFIG_CRYPTO_TEST is not set

    #
    # Authenticated Encryption with Associated Data
    #
    # CONFIG_CRYPTO_CCM is not set
    # CONFIG_CRYPTO_GCM is not set
    # CONFIG_CRYPTO_SEQIV is not set

    #
    # Block modes
    #
    # CONFIG_CRYPTO_CBC is not set
    # CONFIG_CRYPTO_CTR is not set
    # CONFIG_CRYPTO_CTS is not set
    CONFIG_CRYPTO_ECB=y
    # CONFIG_CRYPTO_LRW is not set
    # CONFIG_CRYPTO_PCBC is not set
    # CONFIG_CRYPTO_XTS is not set

    #
    # Hash modes
    #
    # CONFIG_CRYPTO_HMAC is not set
    # CONFIG_CRYPTO_XCBC is not set
    # CONFIG_CRYPTO_VMAC is not set

    #
    # Digest
    #
    # CONFIG_CRYPTO_CRC32C is not set
    # CONFIG_CRYPTO_GHASH is not set
    # CONFIG_CRYPTO_MD4 is not set
    # CONFIG_CRYPTO_MD5 is not set
    # CONFIG_CRYPTO_MICHAEL_MIC is not set
    # CONFIG_CRYPTO_RMD128 is not set
    # CONFIG_CRYPTO_RMD160 is not set
    # CONFIG_CRYPTO_RMD256 is not set
    # CONFIG_CRYPTO_RMD320 is not set
    # CONFIG_CRYPTO_SHA1 is not set
    # CONFIG_CRYPTO_SHA256 is not set
    # CONFIG_CRYPTO_SHA512 is not set
    # CONFIG_CRYPTO_TGR192 is not set
    # CONFIG_CRYPTO_WP512 is not set

    #
    # Ciphers
    #
    CONFIG_CRYPTO_AES=y
    # CONFIG_CRYPTO_ANUBIS is not set
    CONFIG_CRYPTO_ARC4=y
    # CONFIG_CRYPTO_BLOWFISH is not set
    # CONFIG_CRYPTO_CAMELLIA is not set
    # CONFIG_CRYPTO_CAST5 is not set
    # CONFIG_CRYPTO_CAST6 is not set
    # CONFIG_CRYPTO_DES is not set
    # CONFIG_CRYPTO_FCRYPT is not set
    # CONFIG_CRYPTO_KHAZAD is not set
    # CONFIG_CRYPTO_SALSA20 is not set
    # CONFIG_CRYPTO_SEED is not set
    # CONFIG_CRYPTO_SERPENT is not set
    # CONFIG_CRYPTO_TEA is not set
    # CONFIG_CRYPTO_TWOFISH is not set

    #
    # Compression
    #
    # CONFIG_CRYPTO_DEFLATE is not set
    # CONFIG_CRYPTO_ZLIB is not set
    # CONFIG_CRYPTO_LZO is not set

    #
    # Random Number Generation
    #
    # CONFIG_CRYPTO_ANSI_CPRNG is not set
    # CONFIG_CRYPTO_HW is not set
    # CONFIG_BINARY_PRINTF is not set

    #
    # Library routines
    #
    CONFIG_BITREVERSE=y
    CONFIG_GENERIC_FIND_LAST_BIT=y
    CONFIG_CRC_CCITT=m
    # CONFIG_CRC16 is not set
    CONFIG_CRC_T10DIF=m
    # CONFIG_CRC_ITU_T is not set
    CONFIG_CRC32=y
    # CONFIG_CRC7 is not set
    # CONFIG_LIBCRC32C is not set
    CONFIG_ZLIB_INFLATE=y
    CONFIG_ZLIB_DEFLATE=y
    CONFIG_DECOMPRESS_GZIP=y
    CONFIG_GENERIC_ALLOCATOR=y
    CONFIG_HAS_IOMEM=y
    CONFIG_HAS_IOPORT=y
    CONFIG_HAS_DMA=y
    CONFIG_NLATTR=y
    CONFIG_GENERIC_ATOMIC64=y

    ---------------------------------------------------------------------------

    Thanks again for you two guys suggestion.

    Regards, James

  • Sounds like you got it working. All the gadgets need an HCD driver to function. I would guess your kernel was compiled without it. I think the UVC option disappears  because you have forced device-only mode. The UVC option needs target as a host? That's my guess. Judging from the Kconfig files, you should only need to include "Video  For Linux" to enable the "USB Webcam Gadget".