This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to create boot.scr script for AM3715 with 5.02 SDK? And why VFS cannot open root device?



Dear Sir/Lady,

I compile the MLO, u-boot.bin and uImage without problem (applied 5.02 SDK linux with beagle-xm configuration). But I don't know how to create the boot.scr script for my project. Here is the environment info (using "pri" under u-boot prompt):

Texas Instruments X-Loader 1.51 (Aug 24 2012 - 14:24:16)
Unsupported Chip!
Beagle xM Rev A


UNICORN-Robert-SHEEPBOARD test build--Rev:02-----------------------

Starting X-loader on MMC
Reading boot sector

219156 Bytes Read from MMC
Starting OS Bootloader from MMC...
Starting OS Bootloader...


U-Boot 2010.06 (Aug 24 2012 - 15:44:44)

OMAP34xx/35xx-GP ES2.1, CPU-OPP2 L3-165MHz
OMAP3 Beagle board + LPDDR/NAND
I2C: ready
RAM Configuration:
Bank #0: 80000000 512 MiB
Bank #1: a0000000 0 Bytes
DRAM: 512 MiB
NAND: HW ECC [Kernel/FS layout] selected
NAND device: Manufacturer ID: 0x2c, Chip ID: 0xdc (Micron NAND 512MiB 3,3V 8-bit
)
NAND bus width 16 instead 8 bit
0 MiB
*** Warning - bad CRC or NAND, using default environment

In: serial
Out: serial
Err: serial
Beagle unknown 0x02
Die ID #3e2c00029e3800000168263d1802b01f
Hit any key to stop autoboot: 0
mmc1 is available
reading boot.scr

464 bytes read
Running bootscript from mmc ...
## Executing script at 82000000
syntax error
OMAP3 beagleboard.org # pri
bootcmd=if mmc init; then if run loadbootscript; then run bootscript; else if ru
n loaduimage; then run mmcboot; else run nandboot; fi; fi; else run nandboot; fi
bootdelay=10
baudrate=115200
loadaddr=0x82000000
usbtty=cdc_acm
console=ttyO2,115200n8
mpurate=500
vram=12M
dvimode=1024x768MR-16@60
defaultdisplay=dvi
mmcroot=/dev/mmcblk0p2 rw
mmcrootfstype=ext3 rootwait
nandroot=/dev/mtdblock4 rw
nandrootfstype=jffs2
mmcargs=setenv bootargs console=${console} mpurate=${mpurate} vram=${vram} omapf
b.mode=dvi:${dvimode} omapdss.def_disp=${defaultdisplay} root=${mmcroot} rootfst
ype=${mmcrootfstype}
nandargs=setenv bootargs console=${console} mpurate=${mpurate} vram=${vram} omap
fb.mode=dvi:${dvimode} omapdss.def_disp=${defaultdisplay} root=${nandroot} rootf
stype=${nandrootfstype}
loadbootscript=fatload mmc 0 ${loadaddr} boot.scr
bootscript=echo Running bootscript from mmc ...; source ${loadaddr}
loaduimage=fatload mmc 0 ${loadaddr} uImage
mmcboot=echo Booting from mmc ...; run mmcargs; bootm ${loadaddr}
nandboot=echo Booting from nand ...; run nandargs; nand read ${loadaddr} 280000
400000; bootm ${loadaddr}
stdin=serial
stdout=serial
stderr=serial
dieid#=3e2c00029e3800000168263d1802b01f
filesize=1D0

Environment size: 1208/131068 bytes
OMAP3 beagleboard.org #

When I ignore the boot.scr file (no boot.scr in SD card), the kernel will be loaded, and then panic on VFS mount error. 

Please see the log below for more detail:

Texas Instruments X-Loader 1.51 (Aug 24 2012 - 14:24:16)
Unsupported Chip!
Beagle xM Rev A


UNICORN-Robert-SHEEPBOARD test build--Rev:02-----------------------

Starting X-loader on MMC
Reading boot sector

219156 Bytes Read from MMC
Starting OS Bootloader from MMC...
Starting OS Bootloader...


U-Boot 2010.06 (Aug 24 2012 - 15:44:44)

OMAP34xx/35xx-GP ES2.1, CPU-OPP2 L3-165MHz
OMAP3 Beagle board + LPDDR/NAND
I2C: ready
RAM Configuration:
Bank #0: 80000000 512 MiB
Bank #1: a0000000 0 Bytes
DRAM: 512 MiB
NAND: HW ECC [Kernel/FS layout] selected
NAND device: Manufacturer ID: 0x2c, Chip ID: 0xdc (Micron NAND 512MiB 3,3V 8-bit
)
NAND bus width 16 instead 8 bit
0 MiB
*** Warning - bad CRC or NAND, using default environment

In: serial
Out: serial
Err: serial
Beagle unknown 0x02
Die ID #13c600029e3800000168263d18025021
Hit any key to stop autoboot: 0
mmc1 is available
reading boot.scr
Invalid FAT entry

** Unable to read "boot.scr" from mmc 0:1 **
reading uImage

3118960 bytes read
Booting from mmc ...
## Booting kernel from Legacy Image at 82000000 ...
Image Name: Linux-2.6.37
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 3118896 Bytes = 3 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK

Starting kernel ...

Uncompressing Linux... done, booting the kernel.
[ 0.000000] Linux version 2.6.37 (ubuntu@ubuntu) (gcc version 4.3.3 (GCC) ) #
1 Fri Aug 24 16:45:57 CST 2012
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f
[ 0.000000] CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] Machine: OMAP3 Beagle Board
[ 0.000000] Reserving 12582912 bytes SDRAM for VRAM
[ 0.000000] Memory policy: ECC disabled, Data cache writeback
[ 0.000000] OMAP3630 ES1.2 (l2cache sgx neon isp 192mhz_clk )
[ 0.000000] SRAM: Mapped pa 0x40200000 to va 0xfe400000 size: 0x10000
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pag
es: 126976
[ 0.000000] Kernel command line: console=ttyO2,115200n8 mpurate=500 vram=12M
omapfb.mode=dvi:1024x768MR-16@60 omapdss.def_disp=dvi root=/dev/mmcblk0p2 rw roo
tfstype=ext3 rootwait
[ 0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Memory: 500MB = 500MB total
[ 0.000000] Memory: 493996k/493996k available, 30292k reserved, 0K highmem
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
[ 0.000000] DMA : 0xffc00000 - 0xffe00000 ( 2 MB)
[ 0.000000] vmalloc : 0xe0800000 - 0xf8000000 ( 376 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xe0000000 ( 512 MB)
[ 0.000000] modules : 0xbf000000 - 0xc0000000 ( 16 MB)
[ 0.000000] .init : 0xc0008000 - 0xc003d000 ( 212 kB)
[ 0.000000] .text : 0xc003d000 - 0xc05d15fc (5714 kB)
[ 0.000000] .data : 0xc05d2000 - 0xc078e020 (1777 kB)
[ 0.000000] NR_IRQS:409
[ 0.000000] Clocking rate (Crystal/Core/MPU): 26.0/400/600 MHz
[ 0.000000] omap_hwmod: i2c1: softreset failed (waited 10000 usec)
[ 0.000000] omap_hwmod: i2c2: softreset failed (waited 10000 usec)
[ 0.000000] omap_hwmod: i2c3: softreset failed (waited 10000 usec)
[ 0.000000] Reprogramming SDRC clock to 400000000 Hz
[ 0.000000] dpll3_m2_clk rate change failed: -22
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 4.0) with 96 interrupt
s
[ 0.000000] Total of 96 interrupts on 1 active controller
[ 0.000000] GPMC revision 5.0
[ 0.000000] Trying to install interrupt handler for IRQ402
[ 0.000000] Trying to install interrupt handler for IRQ403
[ 0.000000] Trying to install interrupt handler for IRQ404
[ 0.000000] Trying to install interrupt handler for IRQ405
[ 0.000000] Trying to install interrupt handler for IRQ406
[ 0.000000] Trying to install interrupt handler for IRQ407
[ 0.000000] Trying to install interrupt handler for IRQ408
[ 0.000000] Trying to install type control for IRQ409
[ 0.000000] Trying to set irq flags for IRQ409
[ 0.000000] OMAP clockevent source: GPTIMER12 at 32768 Hz
[ 0.000000] Console: colour dummy device 80x30
[ 0.000000] Lock dependency validator: Copyright (c) 2006 Red Hat, Inc., Ingo
Molnar
[ 0.000000] ... MAX_LOCKDEP_SUBCLASSES: 8
[ 0.000000] ... MAX_LOCK_DEPTH: 48
[ 0.000000] ... MAX_LOCKDEP_KEYS: 8191
[ 0.000000] ... CLASSHASH_SIZE: 4096
[ 0.000000] ... MAX_LOCKDEP_ENTRIES: 16384
[ 0.000000] ... MAX_LOCKDEP_CHAINS: 32768
[ 0.000000] ... CHAINHASH_SIZE: 16384
[ 0.000000] memory used by lock dependency info: 3951 kB
[ 0.000000] per task-struct memory footprint: 2304 bytes
[ 0.000000] Calibrating delay loop... 500.97 BogoMIPS (lpj=1953792)
[ 0.000000] pid_max: default: 32768 minimum: 301
[ 0.000000] Security Framework initialized
[ 0.000000] Mount-cache hash table entries: 512
[ 0.000000] CPU: Testing write buffer coherency: ok
[ 0.000000] regulator: core version 0.5
[ 0.000000] regulator: dummy:
[ 0.000000] NET: Registered protocol family 16
[ 0.000000] OMAP GPIO hardware version 2.5
[ 0.000000] OMAP GPIO hardware version 2.5
[ 0.000000] OMAP GPIO hardware version 2.5
[ 0.000000] OMAP GPIO hardware version 2.5
[ 0.000000] OMAP GPIO hardware version 2.5
[ 0.000000] OMAP GPIO hardware version 2.5
[ 0.000000] omap_mux_init: Add partition: #1: core, flags: 0
[ 0.000000] OMAP3 Beagle Rev: unknown 2
[ 0.000000] Found NAND on CS0
[ 0.000000] Registering NAND on CS0
[ 0.000000] Unable to get DVI reset GPIO
[ 0.000000] hw-breakpoint: debug architecture 0x4 unsupported.
[ 0.000000] Switched to new clocking rate (Crystal/Core/MPU): 26.0/400/500 MH
z
[ 0.000000] OMAP DMA hardware revision 5.0
[ 0.122070] bio: create slab <bio-0> at 0
[ 0.131408] SCSI subsystem initialized
[ 0.143310] usbcore: registered new interface driver usbfs
[ 0.144287] usbcore: registered new interface driver hub
[ 0.145507] usbcore: registered new device driver usb
[ 0.148681] omap_device: omap_i2c.1: new worst case activate latency 0: 30517
[ 0.159606] omap_i2c omap_i2c.1: bus 1 rev4.0 at 2600 kHz
[ 0.172546] twl4030: PIH (irq 7) chaining IRQs 368..375
[ 0.172760] twl4030: power (irq 373) chaining IRQs 376..383
[ 0.175476] twl4030: gpio (irq 368) chaining IRQs 384..401
[ 0.189697] regulator: VMMC1: 1850 <--> 3150 mV at 3000 mV normal standby
[ 0.192871] regulator: VDAC: 1800 mV normal standby
[ 0.196136] regulator: VDVI: 1800 mV normal standby
[ 0.199798] regulator: VSIM: 1800 <--> 3000 mV at 1800 mV normal standby
[ 0.202972] regulator: VAUX3: 1800 mV normal standby
[ 0.206329] regulator: VAUX4: 1800 mV normal standby
[ 0.206848] omap_device: omap_i2c.1: new worst case deactivate latency 0: 305
17
[ 0.218200] omap_i2c omap_i2c.2: bus 2 rev4.0 at 400 kHz
[ 0.231231] omap_i2c omap_i2c.3: bus 3 rev4.0 at 100 kHz
[ 0.239776] Advanced Linux Sound Architecture Driver Version 1.0.23.
[ 0.244445] Switching to clocksource 32k_counter
[ 0.394592] musb-hdrc: version 6.0, otg (peripheral+host), debug=0
[ 0.396209] NET: Registered protocol family 2
[ 0.397033] IP route cache hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.399047] TCP established hash table entries: 16384 (order: 5, 131072 bytes
)
[ 0.399871] TCP bind hash table entries: 16384 (order: 7, 720896 bytes)
[ 0.411102] TCP: Hash tables configured (established 16384 bind 16384)
[ 0.411224] TCP reno registered
[ 0.411254] UDP hash table entries: 256 (order: 2, 24576 bytes)
[ 0.411651] UDP-Lite hash table entries: 256 (order: 2, 24576 bytes)
[ 0.412902] NET: Registered protocol family 1
[ 0.414581] RPC: Registered udp transport module.
[ 0.414611] RPC: Registered tcp transport module.
[ 0.414642] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.415802] NetWinder Floating Point Emulator V0.97 (double precision)
[ 0.418762] omap_init_opp_table: no hwmod or odev for iva, [6] cannot add OPP
s.
[ 0.422058] omap-iommu omap-iommu.0: isp registered
[ 0.423126] AM37x/DM37x Linux PSP version 04.02.00.07 (OMAP3BEAGLE)
[ 0.616241] VFS: Disk quotas dquot_6.5.2
[ 0.616394] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 0.619323] JFFS2 version 2.2. (NAND) (SUMMARY) © 2001-2006 Red Hat, Inc.
[ 0.620666] msgmni has been set to 964
[ 0.625457] io scheduler noop registered
[ 0.625488] io scheduler deadline registered
[ 0.625732] io scheduler cfq registered (default)
[ 0.690124] OMAP DSS rev 2.0
[ 0.690704] OMAP DISPC rev 3.0
[ 0.690856] OMAP VENC rev 2
[ 0.692169] OMAP DSI rev 1.0
[ 1.021484] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[ 1.031127] omap_uart.0: ttyO0 at MMIO 0x4806a000 (irq = 72) is a OMAP UART0
[ 1.033355] omap_uart.1: ttyO1 at MMIO 0x4806c000 (irq = 73) is a OMAP UART1
[ 1.035125] omap_uart.2: ttyO2 at MMIO 0x49020000 (irq = 74) is a OMAP UART2
[ 1.767150] console [ttyO2] enabled
[ 1.772918] omap_uart.3: ttyO3 at MMIO 0x49042000 (irq = 80) is a OMAP UART3
[ 1.833343] brd: module loaded
[ 1.862213] loop: module loaded
[ 1.872894] mtdoops: mtd device (mtddev=name/number) must be supplied
[ 1.879791] omap2-nand driver initializing
[ 1.884674] ONFI flash detected
[ 1.888275] NAND device: Manufacturer ID: 0x2c, Chip ID: 0xdc (Micron )
[ 1.895294] Creating 5 MTD partitions on "omap2-nand.0":
[ 1.900909] 0x000000000000-0x000000080000 : "X-Loader"
[ 1.916778] 0x000000080000-0x000000260000 : "U-Boot"
[ 1.929992] 0x000000260000-0x000000280000 : "U-Boot Env"
[ 1.942962] 0x000000280000-0x000000680000 : "Kernel"
[ 1.957275] 0x000000680000-0x000020000000 : "File System"
[ 2.203460] OneNAND driver initializing
[ 2.214233] usbcore: registered new interface driver asix
[ 2.220672] usbcore: registered new interface driver cdc_ether
[ 2.227630] usbcore: registered new interface driver net1080
[ 2.234375] usbcore: registered new interface driver cdc_subset
[ 2.241363] usbcore: registered new interface driver zaurus
[ 2.247283] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 2.254547] ehci-omap.0 supply hsusb0 not found, using dummy regulator
[ 2.261596] ehci-omap.0 supply hsusb1 not found, using dummy regulator
[ 4.283752] ehci-omap ehci-omap.0: OMAP-EHCI Host Controller
[ 4.292144] ehci-omap ehci-omap.0: new USB bus registered, assigned bus numbe
r 1
[ 4.300537] ehci-omap ehci-omap.0: irq 77, io mem 0x48064800
[ 4.315032] ehci-omap ehci-omap.0: USB 2.0 started, EHCI 1.00
[ 4.322448] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[ 4.329620] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=
1
[ 4.337188] usb usb1: Product: OMAP-EHCI Host Controller
[ 4.342773] usb usb1: Manufacturer: Linux 2.6.37 ehci_hcd
[ 4.348449] usb usb1: SerialNumber: ehci-omap.0
[ 4.359802] hub 1-0:1.0: USB hub found
[ 4.364074] hub 1-0:1.0: 3 ports detected
[ 4.401855] Initializing USB Mass Storage driver...
[ 4.407958] usbcore: registered new interface driver usb-storage
[ 4.414337] USB Mass Storage support registered.
[ 4.420104] usbcore: registered new interface driver usbtest
[ 4.429656] mice: PS/2 mouse device common for all mice
[ 4.438629] input: gpio-keys as /devices/platform/gpio-keys/input/input0
[ 4.454986] omap_device: omap_i2c.1: new worst case activate latency 0: 91552
[ 4.464874] input: twl4030_pwrbutton as /devices/platform/omap/omap_i2c.1/i2c
-1/1-0049/twl4030_pwrbutton/input/input1
[ 4.482452] twl_rtc twl_rtc: rtc core: registered twl_rtc as rtc0
[ 4.489410] twl_rtc twl_rtc: Power up reset detected.
[ 4.495605] twl_rtc twl_rtc: Enabling TWL-RTC.
[ 4.502288] i2c /dev entries driver
[ 4.513275] Linux media interface: v0.10
[ 4.518341] Linux video capture interface: v2.00
[ 4.525268] omap3isp supply VDD_CSIPHY1 not found, using dummy regulator
[ 4.532470] omap3isp supply VDD_CSIPHY2 not found, using dummy regulator
[ 4.540069] omap3isp omap3isp: Revision 15.0 found
[ 4.545471] omap-iommu omap-iommu.0: isp: version 1.1
[ 4.623504] mt9v113 2-003c: chip id mismatch read 0x0, expecting 0x2280
[ 4.638885] isp_register_subdev_group: Unable to register subdev mt9v113
[ 4.647796] usbcore: registered new interface driver uvcvideo
[ 4.653839] USB Video Class driver (v1.0.0)
[ 4.658721] omap_device: omap_wdt.-1: new worst case activate latency 0: 3051
7
[ 4.668518] OMAP Watchdog Timer Rev 0x31: initial timeout 60 sec
[ 4.674926] omap_device: omap_wdt.-1: new worst case deactivate latency 0: 30
517
[ 4.684204] twl4030_wdt twl4030_wdt: Failed to register misc device
[ 4.690856] twl4030_wdt: probe of twl4030_wdt failed with error -16
[ 4.716888] usbcore: registered new interface driver usbhid
[ 4.722778] usbhid: USB HID core driver
[ 4.730834] usbcore: registered new interface driver snd-usb-audio
[ 4.740234] ALSA device list:
[ 4.743316] No soundcards found.
[ 4.746948] oprofile: hardware counters not available
[ 4.752258] oprofile: using timer interrupt.
[ 4.757293] TCP cubic registered
[ 4.760742] Initializing XFRM netlink socket
[ 4.765411] NET: Registered protocol family 17
[ 4.770263] NET: Registered protocol family 15
[ 4.775543] Registering the dns_resolver key type
[ 4.781250] VFP support v0.3: implementor 41 architecture 3 part 30 variant c
rev 3
[ 4.790924] ThumbEE CPU extension supported.
[ 4.814788] Power Management for TI OMAP3.
[ 4.819915] sr_init: No PMIC hook to init smartreflex
[ 4.825744] smartreflex smartreflex.0: omap_sr_probe: SmartReflex driver init
ialized
[ 4.834838] smartreflex smartreflex.1: omap_sr_probe: SmartReflex driver init
ialized
[ 4.844482] SmartReflex Class3 initialized
[ 4.903625] clock: disabling unused clocks to save power
[ 4.917694] fbcvt: 1024x768@60: CVT Name - .786M3-R
[ 4.942565] omap_device: omap_i2c.1: new worst case deactivate latency 0: 610
35
[ 4.950286] regulator_init_complete: incomplete constraints, leaving VDAC on
[ 4.960327] twl_rtc twl_rtc: setting system clock to 2000-01-01 00:00:00 UTC
(946684800)
[ 4.969238] omap_vout omap_vout: Buffer Size = 3686400
[ 4.979156] omap_vout omap_vout: : registered and initialized video device 15
[ 4.986663] omap_vout omap_vout: Buffer Size = 3686400
[ 4.994384] omap_vout omap_vout: : registered and initialized video device 16
[ 5.007049] Waiting for root device /dev/mmcblk0p2...
[ 5.330718] mmc0: new high speed SDHC card at address b368
[ 5.339294] mmcblk0: mmc0:b368 NCard 7.46 GiB (ro)
[ 5.352783] mmcblk0: p1 p2 p3
[ 5.449279] VFS: Cannot open root device "mmcblk0p2" or unknown-block(179,2)
[ 5.456726] Please append a correct "root=" boot option; here are the availab
le partitions:
[ 5.465576] 1f00 512 mtdblock0 (driver?)
[ 5.470886] 1f01 1920 mtdblock1 (driver?)
[ 5.476226] 1f02 128 mtdblock2 (driver?)
[ 5.481567] 1f03 4096 mtdblock3 (driver?)
[ 5.486877] 1f04 517632 mtdblock4 (driver?)
[ 5.492187] b300 7829504 mmcblk0 driver: mmcblk
[ 5.497772] b301 72261 mmcblk0p1 00000000-0000-0000-0000-00000000
0mmcblk0p1
[ 5.506164] b302 923737 mmcblk0p2 00000000-0000-0000-0000-00000000
0mmcblk0p2
[ 5.514587] b303 6811560 mmcblk0p3 00000000-0000-0000-0000-00000000
0mmcblk0p3
[ 5.522979] Kernel panic - not syncing: VFS: Unable to mount root fs on unkno
wn-block(179,2)
[ 5.531860] [<c004daf0>] (unwind_backtrace+0x0/0xec) from [<c04379c0>] (panic
+0x4c/0x184)
[ 5.540710] [<c04379c0>] (panic+0x4c/0x184) from [<c00091f0>] (mount_block_ro
ot+0x1d4/0x21c)
[ 5.549560] [<c00091f0>] (mount_block_root+0x1d4/0x21c) from [<c00092dc>] (mo
unt_root+0xa4/0xc4)
[ 5.558776] [<c00092dc>] (mount_root+0xa4/0xc4) from [<c0009460>] (prepare_na
mespace+0x164/0x1c8)
[ 5.568084] [<c0009460>] (prepare_namespace+0x164/0x1c8) from [<c0008710>] (k
ernel_init+0x10c/0x150)
[ 5.577636] [<c0008710>] (kernel_init+0x10c/0x150) from [<c0048d10>] (kernel_
thread_exit+0x0/0x8)

  • There are three partitions in your card. Where is your filesystem residing? Is it p1/p2/p3. Please specify the bootargs accordingly. Right now you are specifying p2

  • Hi Renjith,

    The file system is exactly in p2, I'm copy it from TargetNFS and I can see it on Ubuntu. Is there any possibility to cause this issue? Or document?

  • Robert,

    Can you mount the card to your PC and do an ls -l on p2 and send me the log? I'm suspecting permission issues also.

  • Hi Renjith,

    Sure, please see the information below and tell me if any more you need.

    robert@ubuntu:/media/rootfs$ df -hT

    Filesystem Type Size Used Avail Use% Mounted on

    /dev/sda1 ext4 29G 8.6G 19G 32% /
    none devtmpfs 1.5G 368K 1.5G 1% /dev
    none tmpfs 1.5G 252K 1.5G 1% /dev/shm
    none tmpfs 1.5G 108K 1.5G 1% /var/run
    none tmpfs 1.5G 0 1.5G 0% /var/lock
    none tmpfs 1.5G 0 1.5G 0% /lib/init/rw
    /dev/sdb3 ext3 6.4G 143M 6.0G 3% /media/START_HERE
    /dev/sdb2 ext3 888M 504M 340M 60% /media/rootfs
    /dev/sdb1 vfat 70M 17M 54M 24% /media/boot
    robert@ubuntu:/media/rootfs$ ls -l
    total 84
    drwxr-xr-x 2 robert robert 4096 2012-03-28 23:03 bin
    drwxr-xr-x 2 robert robert 4096 2012-03-28 23:02 boot
    drwxr-xr-x 3 robert robert 4096 2012-03-26 04:32 dev
    drwxr-xr-x 37 robert robert 4096 2012-03-28 23:03 etc
    drwxr-xr-x 3 robert robert 4096 2012-03-28 21:02 home
    drwxr-xr-x 5 robert robert 4096 2012-03-26 02:11 lib
    lrwxrwxrwx 1 robert robert 12 2012-09-06 18:00 linuxrc -> /bin/busybox
    drwx------ 2 root root 16384 2012-09-06 17:55 lost+found
    drwxr-xr-x 10 robert robert 4096 2012-03-28 21:02 media
    drwxr-xr-x 3 robert robert 4096 2012-03-28 21:03 mnt
    drwxr-xr-x 3 robert robert 4096 2012-03-28 23:02 opt
    drwxr-xr-x 2 robert robert 4096 2012-03-26 04:32 proc
    drwxr-xr-x 2 robert robert 4096 2012-03-28 23:03 sbin
    drwxr-xr-x 3 robert robert 4096 2012-03-28 21:02 srv
    drwxr-xr-x 2 robert robert 4096 2012-03-26 04:32 sys
    drwxr-xr-x 2 robert robert 4096 2012-03-28 23:03 tmp
    drwxr-xr-x 12 robert robert 4096 2012-03-26 01:58 usr
    drwxr-xr-x 7 robert robert 4096 2012-03-26 01:54 var
    drwxr-xr-x 5 robert robert 4096 2012-03-28 23:03 www
    robert@ubuntu:/media/rootfs$ ls -l /home/robert/ti-sdk-am37x-evm-05.05.00.00/targetNFS/
    total 68
    drwxr-sr-x 2 root root 4096 2012-07-27 23:51 bin
    drwxr-sr-x 2 root root 4096 2012-07-27 23:50 boot
    drwxr-sr-x 3 root root 4096 2012-07-26 09:05 dev
    drwxr-sr-x 37 root root 4096 2012-07-27 23:51 etc
    drwxr-sr-x 3 root root 4096 2012-07-27 21:25 home
    drwxr-sr-x 5 root root 4096 2012-07-26 06:51 lib
    lrwxrwxrwx 1 root root 12 2012-08-31 11:51 linuxrc -> /bin/busybox
    drwxr-sr-x 10 root root 4096 2012-07-27 21:25 media
    drwxr-sr-x 3 root root 4096 2012-07-27 21:25 mnt
    drwxrwsrwx 3 root root 4096 2012-07-27 23:50 opt
    drwxr-sr-x 2 root root 4096 2012-07-26 09:05 proc
    drwxr-sr-x 2 root root 4096 2012-07-27 23:51 sbin
    drwxr-sr-x 3 root root 4096 2012-07-27 21:25 srv
    drwxr-sr-x 2 root root 4096 2012-07-26 09:05 sys
    drwxrwsrwt 2 root root 4096 2012-07-27 23:51 tmp
    drwxr-sr-x 12 root root 4096 2012-07-26 06:24 usr
    drwxr-sr-x 7 root root 4096 2012-07-26 06:21 var
    drwxr-sr-x 5 root root 4096 2012-07-27 23:51 www
    robert@ubuntu:/media/rootfs$

    This is what am I using to copy the file-system:
    "sudo cp -rv ~/ ti-sdk-am37x-evm-05.05.00.00 /targetNFS/* /media/rootfs"

  • Robert,

    In the filesystem there is no init program in the root directory. That's not the problem here at first. 

    Looks the the file system is not detected properly. Can you try the following?

    1. See whether ext3 filesystem support is enabled in the kernel configs?

    2. Are you able to mount the SD card and see the contents when you are booted up in NFS?

    3. Can you re-partition the card and try again?

    4. If this doesn't work, can you send your .config file?

  • Hello Renjith,

    The problem was been solved by our partner. Currently we update the SDK to 05.05 version, and we change a source file "board-omap3beagle.c" which locate "

    robert@ubuntu:~/ti-sdk-am37x-evm-05.05.00.00/board-support/linux-2.6.37-psp04.02.00.07.sdk/arch/arm". Here are detail info about this modify:

    static int beagle_twl_gpio_setup(struct device *dev,
    unsigned gpio, unsigned ngpio)
    {
    if (omap3_beagle_get_rev() == OMAP3BEAGLE_BOARD_XM) {
    mmc[0].gpio_wp = -EINVAL;
    } else if ((omap3_beagle_get_rev() == OMAP3BEAGLE_BOARD_C1_3) ||
    (omap3_beagle_get_rev() == OMAP3BEAGLE_BOARD_C4)) {
    omap_mux_init_gpio(23, OMAP_PIN_INPUT);
    mmc[0].gpio_wp = 23;
    } else {
    omap_mux_init_gpio(29, OMAP_PIN_INPUT);
    }

    mmc[0].gpio_wp = -EINVAL; //Robert add-Sep10-2012


    The root cause in this case may difference board ID and GPIO between EV board and ours. After we insert the above words, now we can step forward to "login" section.

    Thanks anyway for your help, Renjith!