This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP-L138 GPIO peripheral Clock



hello everyone, 

I'm working on EVM OMAP l138 and using Code composer V 5.1 

how could i get the clock value of  the GPIO peripheral and how to change ?

  • if my question is not clear, here  what i faced exactly.

    I'm working on DSP (C6748).

    i have configured GP7[9] as interrupt source (input pin)  to accept clock cycles with period 3300 nanoseconds [Logic 1 period is 320 ns and logic 0 period is 2.9us]

    DSP detects interrupt on Rising Edge and the ISR is as follows :

    if(GPIOPinIntStatus(SOC_GPIO_0_REGS,GPIO7P9)) 
    {

    count++; // count no of  times ISR is executed  
    GPIOPinIntClear(SOC_GPIO_0_REGS, GPIO7P9);
    }

    The problem is

            i have 52 clock cycles each 3300 nanoseconds coming on GP7[9] so that DSP should detects 52 interrupt (which is not the case i have )

            The DSP detects only 50 interrupt so i thought the problem is in GPIO peripheral clock .   

            So i want to know if the problem in GPIO peripheral clock or in something else ? and how to solve it ?

    thanks in advance .