This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INTEL E82575ET can not work

I am working on TI 814X, I connect INTEL  82575ET PCIE ethernet card with PCIE interface.

I can find two ethernet scoket(eth1, eth2) , provied by  INTEL  E82575ET , but ping can not work.

The following is  my steps:

1.
  Device Drivers  --->
             [*] Network device support  --->
                      [*]   Ethernet (1000 Mbit)  --->
                            <M>   Intel(R) 82575/82576 PCI-Express Gigabit Ethernet support
2. find “igb.ko” ,then  " insmod igb.ko  "
3. #ifconfig -a
eth0      Link encap:Ethernet  HWaddr 50:56:63:9E:0D:CA  
          inet addr:192.168.1.3  Bcast:192.168.1.255  Mask:255.255.255.0
          UP BROADCAST MULTICAST  MTU:1500  Metric:1
          RX packets:0 errors:0 dropped:0 overruns:0 frame:0
          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000
          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)
          Interrupt:40

eth1      Link encap:Ethernet  HWaddr 00:1B:57:60:07:D4  
          inet addr:192.168.1.8  Bcast:192.168.1.255  Mask:255.255.255.0
          UP BROADCAST MULTICAST  MTU:1500  Metric:1
          RX packets:0 errors:0 dropped:0 overruns:0 frame:0
          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000
          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)
          Memory:21000000-21020000

eth2      Link encap:Ethernet  HWaddr 00:1B:57:60:07:D5  
          inet addr:192.168.1.9  Bcast:192.168.1.255  Mask:255.255.255.0
          UP BROADCAST MULTICAST  MTU:1500  Metric:1
          RX packets:0 errors:0 dropped:0 overruns:0 frame:0
          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000
          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)
          Memory:21020000-21040000

lo        Link encap:Local Loopback  
          inet addr:127.0.0.0  Mask:255.0.0.0
          UP LOOPBACK RUNNING  MTU:16436  Metric:1
          RX packets:8 errors:0 dropped:0 overruns:0 frame:0
          TX packets:8 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:0
          RX bytes:496 (496.0 B)  TX bytes:496 (496.0 B)