am using a WINEC7. As I know by default RAM registry is used by system, to keep registry information persistent I am trying to use hive based registry. From Catalog item in Platform Builder, I choose hive based registry .
made necessary changes in platform.reg and sdhc.reg file with the help of followings threads
http://social.msdn.microsoft.com/Forums/en-US/winembplatdev/thread/9bdc1c95-a6e8-4f07-a6b2-7fb11c47268f
http://msdn.microsoft.com/en-us/library/ee490032%28v=WinEmbedded.60%29.aspx
http://processors.wiki.ti.com/index.php/Persistent_Registry_in_ARM-A8_BSP#SD.2FMMC_Persistent_Storage
after the compilation when i try to run the image it hangs at +PrcmPostInit()
do we need to add
SD Bus Driver (add to sdhc.reg)
[HKEY_LOCAL_MACHINE\Drivers\BuiltIn\SDBusDriver] and
SDCard Client Drivers (SDMemory_Class, MMC_Class and their High_Capacity versions) (add to sdhc.reg)
[HKEY_LOCAL_MACHINE\Drivers\SDCARD\ClientDrivers\Class\SDMemory_Class]
I hope i get a reply ASAP