Other Parts Discussed in Thread: SYSBIOS
I have ported the UnitTest++ framework to a CCS v.5.1 project running on the DSK 6455. UnitTest++ is an open source unit testing framework for C++. It has a set of self-tests that can be run to determine if the framework itself is operating correctly. Most of the 175 self-tests pass, but there is one failure I would like to ask about.
Without getting into too much detail about how UnitTest++ works, I'll say the failed test is intentionally causing an exception in order to see if the test reports this as a failure condition. A try/catch construct is used to trap the exception. Several of the other self-tests also generate intentional exceptions, and these are handled correctly as expected. But the unique thing about the test in question is that (I suspect) it creates an internal CPU Instruction Fetch exception which apparently cannot be intercepted by the try/catch. Instead, I get the following error message in the console and my application is terminated (note there were a bunch of register values printed too, but I'm not sure it's worth taking up all the space to add them here):
Exception at 0x0
EFR=0x2 NRP=0x[C64XP_0] 0
Internal exception: IERR=0x1
Instruction fetch exception
ti.sysbios.family.c64p.Exception: line 248: E_exceptionMin: pc = 0x0088cf44, sp = 0x0090b1f8.
xdc.runtime.Error.raise: terminating execution
The method used by UnitTest++ to generate the exception is the following line of code:
reinterpret_cast< void (*) () >(0) ();
This code seems to be basically making a function call through a function pointer that is 0. No surprise this generates an exception, but that is what they want to do for the test. I can generate the same error with the following code:
void (*FuncPtr) ();
FuncPtr = 0;
(*FuncPtr) ();
So, finally to my question: is there a way to configure or build my project so the try/catch will catch the exception rather than have it terminate? I looked into perhaps setting up some exception hook function via the Exception module in the xdc tool in hopes I could run my own function instead of the SYS/BIOS Exception_handler() function. I can see in Exception_handler() where it might call my exception hook function. But unfortunately, I can also see that it apparently will still fall through and call Error_raise() which is what terminates my application.
My worst-case solution is to add conditional compiles to the UnitTest++ code so this one test is left out. I can see the UnitTest++ developers have already done this for the MINGW platform. I was just hoping there was some simple way to avoid this on the TI DSP.
Other info about my configuration is as follows:
SYS/BIOS 6.32.5.54
Compiler TI v7.3.1
Output format: COFF Little Endian
XDCtools 3.22.04.46
Linking to rts64plus_eh.lib
Enable C++ exception handling checked
Any information you can provide is appreciated. Thanks.
Jeff Vernon