Other Parts Discussed in Thread: AM3359, SYSBIOS
Hello all,
where can I find a prebuilt binary for the U-Boot to be used on the AM3359 IDK? The board comes with an SD card that is preloaded with various software. I found the MLO and could successfully load and execute the EtherCAT demo app.
What I am really after is to run the QNX Neutrino RTOS on that board. So I need MLO and u-boot.img, which I can then use to load the QNX boot image (via uEnv.txt). We know that this is working on the General Purpose EVM, but the MLO and u-boot.img contained in the corresponding BSP do not work with the IDK.
any help greatly appreciated.
-Albrecht