Hi all,
I'm facing some unexpected issues with a ezdsp5535 that I recently purchased and I hope that someone here might have some help to provide.
I performed the normal CCS4 install (under windows 8 Pro), without the board plugged in and everthing gone perfect. I installed the board drivers and got the demo to work while connecting through J1 perfectly.
However, when I plugg through J2 and try to do some testing using custom code (for example lcd-osd9616) at connection time with the target I get the following error message:
C55xx: Error connecting to the target: (Error -151 @ 0x0) This utility failed to open the adapter for a custom emulator. The adapter returned an error. (Release 5.0.429.0)
I did my setup using TI XDS100v2 USB Emu and EZDSP5535 device. Just to specify that I also have a ezdsp5515 finger print DK, I can perfectly connect and debug with. Also, I tried the install on a Win7 computer with no more luck (as a sanity check for win8 potential issues)
As additional details, the board is recognized in the driver manager as:
- Ports (Com and LPT) --> USB Serial Port (COM7and COM8)
- Universal Serial bus controllers --> USB Serial Converter (A and B)
Which sounds weird to me as I would be expecting TI XDS100 Channel (A and B) in universal.
I spent hours on it already and would greatly appreciate any help before I throw the kit through my window ;-) Kinding but noot that much.
Thank you a lot!
Sincerely,
Jean-Christophe