hello :
I am using SRIO, and I wan to know the SRIO is Full-duplex OR Half-duplex?
I know the most bandwidth of SRIO is 5Gbps*4 = 20Gbps, the 20Gbps is the Sending speed,
1 . if the SRIO is receiving data at the same time it sending data , the SRIO bandwidth should be 20Gbps*2= 40Gbps, Is it right?
2 if SRRIO is sending data and at the same time , it is receiving data from other DSP, Is the Sending speed still 20Gbps?
will the receiving operation affect the Sending Speed ? if the sending operation and the receiving operation are independent?
Thanks