This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Low amplitude while using DMIC input



We are seeing very low amplitude while using the DMIC input for audio recordings, despite setting DMIC1 UL Volume to 29dB. This is on a customer product that has an OMAP4430 running Android Gingerbread, based off of the L27.INC1.13.1 OMAP4 release. Are there any known issues with the audio chain for the DMIC input that would cause very low amplitude in the audio recordings?

Thanks

R.A.Raghuvir