This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

sys_boot pins and resistors

Hi,

I need to modify a prototype board which was done incorrectly. 

Is it OK to connect the OMAP's sys_boot[0:4] pins directly to GND or 1V8 without 10kΩ resistors?  Can I still boot this way?

Thanks for your help.