Other Parts Discussed in Thread: TMS320DM6446
Hi,
I am using dm6446-evm and dvsdk_setuplinux_2_00_00_22. I am able to build dvsdk properly and got encode and decode applications built for dm6446evm.
I am able to boot the evm over nfs.
But the problem is that when i run encode application i get following issue
./encode -v test.264 -o
Encode demo started. Error: Failed to create attribute window device
Error: Failed to create UI
I have set boot arguments as provided in TMS320DM6446 DVEVM v2.0 Getting Started Guide
In my boot log i am see following warning
davincifb davincifb.0: dm_osd0_fb: Failed to obtain ownership of OSD window.
Any help on this will be g8.
Thanks.