Hi
After a long struggle I am able to boot my OMAP L138 EVM kit using 4 GB HDSC Card.
The last few lines of status on TERA TERM are as under, please validate successful booting.
******************************************************************
-OALDumpClocks
-OEMInit
PINMUX14=0x00000000
PINMUX15=0x00000000
PINMUX16=0x22222200
PINMUX17=0x22222222
PINMUX18=0x22000022
PINMUX19=0x02000022
OEMGetExtensionDRAM: Added 0x83E00000 -> 0x88000000
OEM: Cleaning system hive
OEM: Cleaning user profiles
WARN: Updating local copy of BSP_ARGS
OEM: Not cleaning system hive
Adapter's MAC address is 00:08:EE:03:D0:D3
StartupApp: Launching process NAME='xamlperf.exe', CMD='\windows\bounce.xaml'
StartupApp: Process created OK
StartupApp: Process timed out, TA code: 0x1
*****************************************************************************
please confirm....
hemant