This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Two Ethernet MAC with AM335x



At the moment we are evaluating AM335x processor to use in a project where we have a requirement of two Ethernet MAC ports. To be more a little bit more precise, this project requires a Linux operating system with two ethernet interfaces, e.g. eth0 and eth1, working with different MAC addresses. Is this possbile with AM335x processor series ? If yes, which chip has to be used, one with PRU or without ?