Hi,
I am working on Linux-3.0.21-00003-OMAP-Android+ with ICS android on OMAP4430 based custom board.
- When I first start hardware, it successfully boots up.
- Once the system is up running, when I type reboot
command, it restarts the kernel and hangs at
Starting kernel ... Uncompressing Linux... done, booting the kernel.
To debug this issue I compiled the kernel with CONFIG_DEBUG_LL=y
and added few prints.
Now it came to conclusion that kernel read hangs in arc/arm/mach-omap2/omap_hwmod.c,
in function omap_hwmod_read in __raw_readl with clock named aess_fck.
The same thing works on every hard reboot and stucks at the same point on soft reboot.
Please provide some input to solve this issue.