This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

omap3isp omap3isp: isp_wait: wait is too much omap3isp omap3isp: ccdc 1 won't become idle!

Other Parts Discussed in Thread: OMAP3530

Hi,everyone!

I have a DM3730 board, and I want to trasmit some video data to webserver wit GStreamer

the website  is about example GSstreamer pipelines ,http://processors.wiki.ti.com/index.php/Example_GStreamer_Pipelines#OMAP35x

Now,I face a question,as followed:

rameter-sets=(string)\"Z0KAFItoF[18058.919342] pgd = dd4e4000
B8QAA\\=\\=\\,aM4BqHcgAA\\=\\=\"[18058.924743] [287d2484] *pgd=00000000, payload=(int)96, ssrc=(uint)25
72274166, clock-base=(uint)51423[18058.933776] Internal error: Oops: 5 [#3] PREEMPT
[18058.941162] last sysfs file: /sys/devices/virtual/video4linux/video0/dev
[18058.947906] Modules linked in: sdmak lpm_omap3530 dsplinkk cmemk
[18058.953979] CPU: 0    Tainted: G      D     (2.6.32 #4)
[18058.959228] PC is at sg_next+0x0/0x24
[18058.962921] LR is at dma_unmap_sg+0x18/0x28
[18058.967102] pc : [<c01f1134>]    lr : [<c003dc8c>]    psr: 80000013
[18058.967132] sp : dcd65e18  ip : dd466968  fp : 41a3ea14
[18058.978668] r10: 00000000  r9 : dcd64000  r8 : dcd65e64
[18058.983886] r7 : dfa18780  r6 : dd465ec0  r5 : 000000cb  r4 : 00000005
[18058.990447] r3 : 287d2485  r2 : 000000cb  r1 : e0a3b000  r0 : 287d2484
[18058.997009] Flags: Nzcv  IRQs on  FIQs on  Mode SVC_32  ISA ARM  Segment user
[18059.004180] Control: 10c5387d  Table: 9d4e4019  DAC: 00000015
[18059.009948] Process v4l2src0:src (pid: 1556, stack limit = 0xdcd642e8)
[18059.016510] Stack: (0xdcd65e18 to 0xdcd66000)
[18059.020874] 5e00:                                                       dd465f28 dfa18790
[18059.029113] 5e20: dd465ec0 c02c5e70 dd465f28 c02d2c60 dd465ec0 dfa18780 dd4d2800 dfa18790
[18059.037322] 5e40: dcd65e64 c02c42a0 dd4d28b0 dfa18780 dd4d2800 dcd65e64 dfb91cc0 c02d3a5c
[18059.045532] 5e60: dd71e380 00000000 00000001 000ca260 00000000 00000001 00000000 00000000
[18059.053771] 5e80: 41a3e9c4 40722b0c 41a3e9c4 40723d50 00000000 00000002 42c54000 000ca260
[18059.061981] 5ea0: 0011c260 00000070 00000000 00000001 000ca260 00000000 00000001 00000000
[18059.070190] 5ec0: 00000000 41a3e9c4 40722b0c 41a3e9c4 40723d50 00000000 00000002 41b57000
[18059.078399] 5ee0: 000ca260 0011c260 00000070 0000081f c0565e30 c0565f20 0000081f dcd65fb0
[18059.086639] 5f00: dfb91cc0 41a3e97c c0445207 dfb91cc0 41a3e97c c00cae6c dd4520e0 dfb91cc0
[18059.094848] 5f20: 0000000c c00cb54c 000f00d0 c023005c c05b88b8 00000120 00000000 c05b88b8
[18059.103057] 5f40: c05b8960 00000000 00000001 00000048 000f00d0 c0230164 dfa14900 00000000
[18059.111297] 5f60: 00000000 00000048 0000000c 41a3e97c c0445207 dfb91cc0 c0038128 dcd64000
[18059.119506] 5f80: 00000000 c00cb5c8 0000000c 00000001 41a3e97c 00000000 40784a54 41a3ea74
[18059.127716] 5fa0: 00000036 c0037f80 00000000 40784a54 0000000c c0445207 41a3e97c 41a3e97c
[18059.135955] 5fc0: 00000000 40784a54 41a3ea74 00000036 00111788 40798eac 000f00d0 41a3ea14
[18059.144165] 5fe0: 0002ab08 41a3e968 40731064 4050eaec 20000010 0000000c 3c813a80 3c813d7f
[18059.152374] [<c01f1134>] (sg_next+0x0/0x24) from [<c003dc8c>] (dma_unmap_sg+0x18/0x28)
[18059.160339] [<c003dc8c>] (dma_unmap_sg+0x18/0x28) from [<c02c5e70>] (videobuf_dma_unmap+0x4c/0x74)
[18059.169372] [<c02c5e70>] (videobuf_dma_unmap+0x4c/0x74) from [<c02d2c60>] (rsz_vbq_release+0x84/0xec)
[18059.178649] [<c02d2c60>] (rsz_vbq_release+0x84/0xec) from [<c02c42a0>] (videobuf_qbuf+0x258/0x40c)
[18059.187652] [<c02c42a0>] (videobuf_qbuf+0x258/0x40c) from [<c02d3a5c>] (rsz_unlocked_ioctl+0x31c/0x988)
[18059.197082] [<c02d3a5c>] (rsz_unlocked_ioctl+0x31c/0x988) from [<c00cae6c>] (vfs_ioctl+0x2c/0xac)
[18059.206024] [<c00cae6c>] (vfs_ioctl+0x2c/0xac) from [<c00cb54c>] (do_vfs_ioctl+0x570/0x5b8)
[18059.214416] [<c00cb54c>] (do_vfs_ioctl+0x570/0x5b8) from [<c00cb5c8>] (sys_ioctl+0x34/0x54)
[18059.222808] [<c00cb5c8>] (sys_ioctl+0x34/0x54) from [<c0037f80>] (ret_fast_syscall+0x0/0x2c)
[18059.231292] Code: e8bd8ff0 c04e584f c04e9428 c04ee1cc (e5903000)
[18059.239593] omap3isp omap3isp: isp_wait: wait is too much
[18059.245025] omap3isp omap3isp: ccdc 1 won't become idle!
2033, seqnum-base=(uint)43356
/GstPipeline:pipeline0/GstUDPSink[18059.254577] ---[ end trace 3b072a5b48ca7d7e ]---
:udpsink0.GstPad:sink: caps = application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H264, sprop-parameter-sets=(string)\"Z0KAFItoFB8QAA\\=\\=\\,aM4BqHcgAA\\=\\=\", payload=(int)96, ssrc=(uint)2572274166, clock-base=(uint)514232033, seqnum-base=(uint)43356

the question have trobled me for a long time, Hope help!

Thanks,

jay yang