Other Parts Discussed in Thread: TMS320C6727
Hi,
I have gone through the datasheet of TMS320C6727 dsp and its mentioned that the chip contains the program cache along with the internal program/data RAM but I could not find the location of the cache anywhere in the memory specs of the dsp chip. Pls help if anyone knows where and how is the program cache allocated in memory. Also, it is written that the program executes from the cache by default but in the command file shows that the code is given in the .text section of internal RAM. Thus, is there any way to load the program in cache? or to verify that the program is executing from cache?
Thanks in advance.
Anushree