This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

booting problem

Hi all,

I am using Dm-368 leopard board .Since this is my first interaction with the board I am unable to boot.

I am getting the error log as :

Jumping to entry point at 0x81080000.

LSP 2.10 POST BETA RELEASE
VERSION: 2.10.010.03

U-Boot 1.3.4-svn56 (Mar 24 2011 - 13:53:45)

I2C: ready
DRAM: 128 MB
NAND: NAND device: Manufacturer ID: 0x2c, Chip ID: 0xda (Micron NAND 256MiB 3,3
V 8-bit)
Bad block table found at page 131008, version 0x01
Bad block table found at page 130944, version 0x01
256 MiB
In: serial
Out: serial
Err: serial
Ethernet PHY: GENERIC @ 0x00

NAND read: device 0 offset 0xc900000, size 0x800
2048 bytes read: OK
Current WDT flag is 0xffffffff

NAND read: device 0 offset 0xc800000, size 0x800
2048 bytes read: OK
Current firmware update flag is 0xffffffff
Hit any key to stop autoboot: 0

NAND read: device 0 offset 0x800000, size 0x800000
8388608 bytes read: OK

Loading from NAND 256MiB 3,3V 8-bit, offset 0x400000
Image Name: Linux-2.6.18_pro500-davinci
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 1858436 Bytes = 1.8 MB
Load Address: 80008000
Entry Point: 80008000
## Booting kernel from Legacy Image at 80700000 ...
Image Name: Linux-2.6.18_pro500-davinci
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 1858436 Bytes = 1.8 MB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK

Starting kernel ...

Uncompressing Linux.............................................................
............................................................... done, booting th
e kernel.
Linux version 2.6.18_pro500-davinci (renxiang@renxiang-desktop) (gcc version 4.2
.0 (MontaVista 4.2.0-16.0.32.0801914 2008-08-30)) #1 PREEMPT Sun May 23 21:06:24
PDT 2010
CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177
Machine: DaVinci DM365 IPNC
Memory policy: ECC disabled, Data cache writeback
DaVinci DM0365 variant 0x8
PLL0: fixedrate: 24000000, commonrate: 121500000, vpssrate: 243000000
PLL0: vencrate_sd: 27000000, ddrrate: 243000000 mmcsdrate: 121500000
PLL1: armrate: 297000000, voicerate: 99000000, vencrate_hd: 74250000
CPU0: D VIVT write-back cache
CPU0: I cache: 16384 bytes, associativity 4, 32 byte lines, 128 sets
CPU0: D cache: 8192 bytes, associativity 4, 32 byte lines, 64 sets
Built 1 zonelists. Total pages: 29696
Kernel command line: mem=116M console=ttyS0,115200n8 root=/dev/ram0 rw initrd=0x
82000000,8M ip=off video=davincifb:vid0=OFF:vid1=OFF:osd0=1280x720x16,8000K dm36
5_imp.oper_mode=0 davinci_capture.device_type=4
Unknown boot option `dm365_imp.oper_mode=0': ignoring
Unknown boot option `davinci_capture.device_type=4': ignoring
PID hash table entries: 512 (order: 9, 2048 bytes)
Clock event device timer0_0 configured with caps set: 07
Console: colour dummy device 80x30
Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)
Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)
Memory: 116MB = 116MB total
Memory: 105344KB available (3181K code, 653K data, 184K init)
Security Framework v1.0.0 initialized
Capability LSM initialized
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
checking if image is initramfs...it isn't (bad gzip magic numbers); looks like a
n initrd
Freeing initrd memory: 8192K
NET: Registered protocol family 16
DaVinci: 104 gpio irqs
MUX: initialized GPIO20
MUX: initialized I2C_SCL
MUX: initialized GPIO87
Generic PHY: Registered new driver
ch0 default output "COMPOSITE", mode "NTSC"
VPBE Encoder Initialized
SCSI subsystem initialized
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 4096 (order: 2, 16384 bytes)
TCP bind hash table entries: 2048 (order: 1, 8192 bytes)
TCP: Hash tables configured (established 4096 bind 2048)
TCP reno registered
VFS: Disk quotas dquot_6.5.1
Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
squashfs: version 3.1 (2006/08/19) Phillip Lougher
JFFS2 version 2.2. (NAND) (C) 2001-2006 Red Hat, Inc.
yaffs May 23 2010 21:02:19 Installing.
SGI XFS with no debug enabled
Initializing Cryptographic API
io scheduler noop registered
io scheduler anticipatory registered (default)
LTT : ltt-facilities init
LTT : ltt-facility-core init in kernel
DAVINCI-WDT: DaVinci Watchdog Timer: heartbeat 60 sec
Serial: 8250/16550 driver $Revision: 1.90 $ 2 ports, IRQ sharing disabled
serial8250.0: ttyS0 at MMIO map 0x1c20000 mem 0xfbc20000 (irq = 40) is a 16550A
serial8250.0: ttyS1 at MMIO map 0x1d06000 mem 0xfbd06000 (irq = 41) is a 16550A
RAMDISK driver initialized: 1 RAM disks of 32768K size 1024 blocksize
Davinci EMAC MII Bus: probed
MAC address is deadbeaf
TI DaVinci EMAC Linux version updated 4.0
netconsole: not configured, aborting
Linux video capture interface: v2.00
Trying to register davinci display video device.
layer=c29eae00,layer->video_dev=c29eaf60
Trying to register davinci display video device.
layer=c29eac00,layer->video_dev=c29ead60
davinci_init:DaVinci V4L2 Display Driver V1.0 loaded
i2c /dev entries driver
nand_davinci nand_davinci.0: Using 4-bit hardware ECC
NAND device: Manufacturer ID: 0x2c, Chip ID: 0xda (Micron NAND 256MiB 3,3V 8-bit
)
Creating 5 MTD partitions on "nand_davinci.0":
0x00000000-0x00080000 : "bootloader"
0x00080000-0x00200000 : "params"
0x00200000-0x00400000 : "kernel"
0x00400000-0x01c00000 : "filesystem1"
0x01c00000-0x10000000 : "filesystem2"
nand_davinci nand_davinci.0: hardware revision: 2.3
musb_hdrc: version 6.0, cppi-dma, peripheral, debug=0
musb_hdrc musb_hdrc: No DMA interrupt line
musb_hdrc: USB Peripheral mode controller at c7866000 using DMA, IRQ 12
rtc_davinci_dm365 rtc_davinci_dm365.0: rtc intf: proc
rtc_davinci_dm365 rtc_davinci_dm365.0: rtc intf: dev (254:0)
rtc_davinci_dm365 rtc_davinci_dm365.0: rtc core: registered rtc_davinci_dm365 as
rtc0
rtc wait time out !!!!!
rtc wait time out !!!!!
rtc wait time out !!!!!
rtc wait time out !!!!!
rtc wait time out !!!!!
rtc wait time out !!!!!
rtc wait time out !!!!!
davinci-mmc davinci-mmc.0: Supporting 4-bit mode
davinci-mmc davinci-mmc.0: Using DMA mode
Advanced Linux Sound Architecture Driver Version 1.0.12rc1 (Thu Jun 22 13:55:50
2006 UTC).
ASoC version 0.13.1
CQ0093 Voice Codec 0.1
asoc: cq93vc <-> davinci-vcif mapping ok
ALSA device list:
#0: On-chip voice codec (cq93vc)
IPv4 over IPv4 tunneling driver
TCP bic registered
NET: Registered protocol family 1
NET: Registered protocol family 17
rtc wait time out !!!!!
rtc wait time out !!!!!
rtc wait time out !!!!!
rtc wait time out !!!!!
rtc wait time out !!!!!
rtc wait time out !!!!!
rtc wait time out !!!!!
rtc wait time out !!!!!
rtc wait time out !!!!!
rtc wait time out !!!!!
rtc wait time out !!!!!
rtc wait time out !!!!!
rtc wait time out !!!!!
rtc wait time out !!!!!
rtc wait time out !!!!!
rtc wait time out !!!!!
rtc wait time out !!!!!
rtc wait time out !!!!!
rtc wait time out !!!!!
rtc wait time out !!!!!
rtc wait time out !!!!!
rtc wait time out !!!!!
rtc wait time out !!!!!
rtc wait time out !!!!!
rtc wait time out !!!!!
rtc wait time out !!!!!
Time: timer0_1 clocksource has been installed.
Clock event device timer0_0 configured with caps set: 08
Switched to high resolution mode on CPU 0
rtc_davinci_dm365 rtc_davinci_dm365.0: setting the system clock to 2000-09-14 01
:01:01 (968893261)
RAMDISK: Couldn't find valid RAM disk image starting at 0.
yaffs: dev is 1048576 name is "ram0"
yaffs: Attempting MTD mount on 1.0, "ram0"
yaffs: dev is 1048576 name is "ram0"
yaffs: Attempting MTD mount on 1.0, "ram0"
XFS: bad magic number
XFS: SB validate failed
No filesystem could mount root, tried: ext3 ext2 cramfs squashfs msdos vfat yaf
fs yaffs2 xfs
Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(1,0)

Thanks and Regards.