Other Parts Discussed in Thread: DM3730
Hi,
kernel 2.6.37 /EVM/DM3730
I plan to use usbhost and I come to grips with some problems with power management.
Usbhost clocks prevent CORE retention in idle mode (dynamic power saving) and and if usb clocks are cut it is unstable
- sometimes usbhost1_48m_fck can't be enabled when usb HS device is connected .
I took a look at kernel 3.6 where I suppose usbhost clocks are managed from linux pm (idle frameowrk) but ehci pm is not ready jet -
usbhost dynamic suspend/idle is switched off.
I wonder if it is possible to use OTG in host mode - from first tests it seems that it works (suspend/resume) but current on 1.8 (IO)
is increased considerably. Also I do not know how the usbhost will behave when remote wakeup will occur.
I need your advice and an information that anyone before has tried to use these functionalities before.
Karol