Other Parts Discussed in Thread: AM3359
i use am3359 design a custom board.when i use sd card to boot it have a problem occur:
[ 1.164733] Waiting for root device /dev/mmcblk0p2...
below is the whole info,and i cant solve it,please,need your help:
U-Boot SPL 2011.09 (Feb 09 2012 - 15:38:59)
Texas Instruments Revision detection unimplemented
Could not probe the EEPROM; something fundamentally wrong on the I2C bus.
read_eeprom() failure
OMAP SD/MMC: 0
reading u-boot.img
reading u-boot.img
U-Boot 2011.09 (Feb 09 2012 - 15:11:31)
I2C: ready
DRAM: 256 MiB
WARNING: Caches not enabled
Could not probe the EEPROM; something fundamentally wrong on the I2C bus.
NAND: HW ECC Hamming Code selected
256 MiB
MMC: OMAP SD/MMC: 0
*** Warning - bad CRC, using default environment
Net: cpsw
Hit any key to stop autoboot: 0
SD/MMC found on device 0
reading uEnv.txt
** Unable to read "uEnv.txt" from mmc 0:1 **
reading uImage
2922160 bytes read
## Booting kernel from Legacy Image at 80007fc0 ...
Image Name: Arago/3.1.0-psp04.06.00.03.sdk/a
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2922096 Bytes = 2.8 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
XIP Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
[ 0.000000] Linux version 3.1.0 (jenkins@sdit-build01) (gcc version 4.5.3 20110311 (prerelease) (GCC) ) #1 Thu Feb 9 14:58:49 CST 2012
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f
[ 0.000000] CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] Machine: am335xevm
[ 0.000000] Memory policy: ECC disabled, Data cache writeback
[ 0.000000] AM335X ES1.0 (neon )
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 65024
[ 0.000000] Kernel command line: console=ttyO0,115200n8 root=/dev/mmcblk0p2 rw rootfstype=ext3 rootwait ip=none
[ 0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
[ 0.000000] Memory: 256MB = 256MB total
[ 0.000000] Memory: 253724k/253724k available, 8420k reserved, 0K highmem
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
[ 0.000000] DMA : 0xffa00000 - 0xffe00000 ( 4 MB)
[ 0.000000] vmalloc : 0xd0800000 - 0xf8000000 ( 632 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xd0000000 ( 256 MB)
[ 0.000000] modules : 0xbf000000 - 0xc0000000 ( 16 MB)
[ 0.000000] .text : 0xc0008000 - 0xc0534000 (5296 kB)
[ 0.000000] .init : 0xc0534000 - 0xc056d000 ( 228 kB)
[ 0.000000] .data : 0xc056e000 - 0xc05c2d80 ( 340 kB)
[ 0.000000] .bss : 0xc05c2da4 - 0xc05fd320 ( 234 kB)
[ 0.000000] NR_IRQS:396
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[ 0.000000] Total of 128 interrupts on 1 active controller
[ 0.000000] OMAP clockevent source: GPTIMER1 at 24000000 Hz
[ 0.000000] OMAP clocksource: GPTIMER2 at 24000000 Hz
[ 0.000000] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 178956ms
[ 0.000000] Console: colour dummy device 80x30
[ 0.000252] Calibrating delay loop... 498.89 BogoMIPS (lpj=2494464)
[ 0.058632] pid_max: default: 32768 minimum: 301
[ 0.058787] Security Framework initialized
[ 0.058911] Mount-cache hash table entries: 512
[ 0.059364] CPU: Testing write buffer coherency: ok
[ 0.064943] print_constraints: dummy:
[ 0.065416] NET: Registered protocol family 16
[ 0.065839] GPMC revision 6.0
[ 0.068434] OMAP GPIO hardware version 0.1
[ 0.071351] omap_l3_smx omap_l3_smx.0: couldn't find resource
[ 0.071983] omap_mux_init: Add partition: #1: core, flags: 0
[ 0.075915] omap_i2c.1: alias fck already exists
[ 0.077914] omap2_mcspi.1: alias fck already exists
[ 0.078202] omap2_mcspi.2: alias fck already exists
[ 0.108230] bio: create slab <bio-0> at 0
[ 0.111092] SCSI subsystem initialized
[ 0.113178] usbcore: registered new interface driver usbfs
[ 0.113610] usbcore: registered new interface driver hub
[ 0.113876] usbcore: registered new device driver usb
[ 0.128784] omap_i2c omap_i2c.1: bus 1 rev4.0 at 100 kHz
[ 0.131430] Advanced Linux Sound Architecture Driver Version 1.0.24.
[ 0.132799] Switching to clocksource gp timer
[ 0.138702] Switched to NOHz mode on CPU #0
[ 0.153967] musb-hdrc: version 6.0, ?dma?, otg (peripheral+host)
[ 0.154198] musb-hdrc musb-hdrc.0: dma type: pio
[ 0.155266] musb-hdrc musb-hdrc.0: USB OTG mode controller at d080a000 using PIO, IRQ 18
[ 0.155481] musb-hdrc musb-hdrc.1: dma type: pio
[ 0.156394] musb-hdrc musb-hdrc.1: USB OTG mode controller at d080c800 using PIO, IRQ 19
[ 0.156892] NET: Registered protocol family 2
[ 0.157131] IP route cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.157488] TCP established hash table entries: 8192 (order: 4, 65536 bytes)
[ 0.157712] TCP bind hash table entries: 8192 (order: 3, 32768 bytes)
[ 0.157848] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.157864] TCP reno registered
[ 0.157882] UDP hash table entries: 256 (order: 0, 4096 bytes)
[ 0.157914] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[ 0.158159] NET: Registered protocol family 1
[ 0.158508] RPC: Registered named UNIX socket transport module.
[ 0.158527] RPC: Registered udp transport module.
[ 0.158540] RPC: Registered tcp transport module.
[ 0.158553] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.158828] NetWinder Floating Point Emulator V0.97 (double precision)
[ 0.172829] VFS: Disk quotas dquot_6.5.2
[ 0.172974] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 0.173738] JFFS2 version 2.2. (NAND) (SUMMARY) 漏 2001-2006 Red Hat, Inc.
[ 0.174130] msgmni has been set to 495
[ 0.175096] io scheduler noop registered
[ 0.175115] io scheduler deadline registered
[ 0.175212] io scheduler cfq registered (default)
[ 0.176327] Could not set LED4 to fully on
[ 0.178344] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[ 0.180531] omap_uart.0: ttyO0 at MMIO 0x44e09000 (irq = 72) is a OMAP UART0
[ 0.659948] console [ttyO0] enabled
[ 0.664342] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
[ 0.672205] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
[ 0.680152] omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3
[ 0.688026] omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4
[ 0.695892] omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5
[ 0.715574] brd: module loaded
[ 0.725348] loop: module loaded
[ 0.728881] i2c-core: driver [tsl2550] using legacy suspend method
[ 0.735432] i2c-core: driver [tsl2550] using legacy resume method
[ 0.741921] at24 1-0051: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[ 0.802852] No daughter card found
[ 0.806486] at24 1-0050: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[ 0.872853] AM335X: EVM Config read fail: -110
[ 0.879593] mtdoops: mtd device (mtddev=name/number) must be supplied
[ 0.886727] omap2-nand driver initializing
[ 0.891289] OneNAND driver initializing
[ 0.897234] CAN device driver interface
[ 0.901246] CAN bus driver for Bosch D_CAN controller 1.0
[ 0.907891] usbcore: registered new interface driver cdc_ether
[ 0.914313] usbcore: registered new interface driver cdc_subset
[ 0.920593] Initializing USB Mass Storage driver...
[ 0.925999] usbcore: registered new interface driver usb-storage
[ 0.932316] USB Mass Storage support registered.
[ 0.937259] musb-hdrc musb-hdrc.1: MUSB HDRC host driver
[ 0.942944] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 1
[ 0.950863] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[ 0.958033] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 0.965645] usb usb1: Product: MUSB HDRC host driver
[ 0.970865] usb usb1: Manufacturer: Linux 3.1.0 musb-hcd
[ 0.976461] usb usb1: SerialNumber: musb-hdrc.1
[ 0.982217] hub 1-0:1.0: USB hub found
[ 0.986231] hub 1-0:1.0: 1 port detected
[ 0.991672] mousedev: PS/2 mouse device common for all mice
[ 0.998981] omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0
[ 1.006021] i2c /dev entries driver
[ 1.012538] OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 1.019577] cpuidle: using governor ladder
[ 1.024586] cpuidle: using governor menu
[ 1.032424] usbcore: registered new interface driver usbhid
[ 1.038347] usbhid: USB HID core driver
[ 1.043631] usbcore: registered new interface driver snd-usb-audio
[ 1.052162] ALSA device list:
[ 1.055352] No soundcards found.
[ 1.058926] oprofile: hardware counters not available
[ 1.064248] oprofile: using timer interrupt.
[ 1.068767] nf_conntrack version 0.5.0 (3964 buckets, 15856 max)
[ 1.075696] ip_tables: (C) 2000-2006 Netfilter Core Team
[ 1.081426] TCP cubic registered
[ 1.084872] NET: Registered protocol family 17
[ 1.089558] can: controller area network core (rev 20090105 abi 8)
[ 1.096188] NET: Registered protocol family 29
[ 1.100864] can: raw protocol (rev 20090105)
[ 1.105372] can: broadcast manager protocol (rev 20090105 t)
[ 1.111369] Registering the dns_resolver key type
[ 1.116414] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 1.124499] ThumbEE CPU extension supported.
[ 1.129898] _regulator_get: mpu.0 supply mpu not found, using dummy regulator
[ 1.137559] omap2_set_init_voltage: Fail set voltage-dpll_mpu_ck(f=500000000 v=1100000)on vddmpu
[ 1.146822] omap2_set_init_voltage: unable to set vdd_mpu
[ 1.155345] omap_rtc omap_rtc: setting system clock to 2000-01-01 00:00:00 UTC (946684800)
[ 1.164733] Waiting for root device /dev/mmcblk0p2...
please help me !!!thanks!!!