Hello,
while trying to reflash NAND on AM3517 board (SP-860 from Adlink), I, it seems, accidentally erased u-boot and now boot process stops before getting to the u-boot prompt
Texas Instruments X-Loader 1.45 (Feb 7 2012 - 17:12:02)
System Boot: 0c!
mfr:ad
id:da
Starting OS Bootloader...
(stops here)
The board is connected to Linux host via USB-serial adapter, DIP switches are set to the manufacturer's default boot sequence "EMAC -> USB -> MMC1 -> NAND"
There's MMC card inserted into the board, with proper images in place (used to boot from it with no problem)
I would greatly appreciate any tips on restoring the system
Thanks,
Michael